STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Trustzone & TouchGFX/GPU2D support

Hi!Trying to get a TouchGFX working with Trustzone has shown itself to be quite the hassle. Although I have worked through a lot of issues already, my latest one has deemed real stubborn.When enabling GPU2D in a trustzone enabled project, the code th...

Tobiasvb by Associate
  • 529 Views
  • 1 replies
  • 0 kudos

DSI Video Mode (RGB888) with ST7703 on STM32U5G9NJ

  uC – STM32U5G9NJH6Q Display – 720 × 720 (ST7703 panel) Display controller – ST7703 MIPI lanes – 2 lanes DSI Host Mode – Video Mode (DSI_VID_MODE_BURST) Pixel format – RGB888 Problem / Symptoms After the initial display setup (LP mode initia...

PAV by Associate
  • 558 Views
  • 0 replies
  • 0 kudos

Resolved! GPU2D NemaGFX on the STM32N6570-DK hangs

Hello,I'm trying to use the GPU2D on the STM32N6570-DK, with NemaGFX.However, the GPU hangs on random functions.Well actually every time the same funtions, but depending on the number of functions to be executed, so it seems it can only execute a lim...

Circle_unfinished_2.jpg RoundedRect_unfinished_2.jpg
Jack3 by Senior III
  • 1206 Views
  • 2 replies
  • 1 kudos

Resolved! Loading a PNG Image from USB

Hello, I would like to know if there are any methods to load PNGs/JPGs from a USB for the stm32 (I am on stm32F7). I currently imported lodepng but, it seems the malloc used by it is way too large for the device. The png I am loading is relatively sm...

Priyank by Senior
  • 1583 Views
  • 2 replies
  • 1 kudos

Change Alpha on each widgets of container

Hi,I have a container with buttons, images and text (around 30).I would like to change the alpha from 255 to 128 of each widget inside the container.On the documentation, it says it it possible with container with FadeAnimator in Mixins :https://supp...

COSEBE_0-1736037012973.png
COSEBE by Senior
  • 5208 Views
  • 15 replies
  • 3 kudos

Resolved! Repeat Button Implementation

Dear all,Can you please help to point me to any of the repeat button implementation example?I have successfully implement the single button with plus and minus but the number target is too big and it is taking too many clicks to get to the target num...