STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! How to limit TouchGFX to 30 fps

I'm using an STM32H7S78-DK with TouchGFX and FreeRTOS. I would like to limit the framerate of the target to 30fps but withouth reducing the LTDC frequency.Basically having the VSYNC fired at 30fpsI've already set the  ((touchgfx::HALSDL2*)&hal)->s...

nico23 by Senior III
  • 226 Views
  • 5 replies
  • 4 kudos

Dynamic Graph Hard Fault with Large Data Points

Hi,I’m working on an STM based UI with multiple dynamic graph widgets on a single screen and running into a hard fault when scaling things up. Right now I have 5 graph widgets, each needing to plot around 700 data points dynamically. However, when I ...

Riya_L by Associate II
  • 120 Views
  • 2 replies
  • 0 kudos