cancel
Showing results for 
Search instead for 
Did you mean: 

Issue with Vector Renderer and Memory Allocation

TerZer
Associate III

 

Hello everyone,

I am trying to use the Vector Renderer to draw lines because it utilizes GPU2D, which offers faster rendering compared to the Canvas. Below is the code I am using for this purpose:

 

void TestWidget::draw(const touchgfx::Rect& invalidatedArea) const
{
    if (numPoints < 2)
    {
        return; // Nothing to draw
    }

    VectorRenderer* vectorRenderer = VectorRenderer::getInstance();
    // Configure the vector renderer
    Rect absoluteRect = getAbsoluteRect();
    vectorRenderer->setup(absoluteRect, invalidatedArea);
    vectorRenderer->setMode(VectorRenderer::STROKE);
    vectorRenderer->setStrokeWidth(lineWidth);
    vectorRenderer->setColor(lineColor);

    touchgfx::Matrix3x3 transformationMatrix;
	transformationMatrix.scale(scale);
	transformationMatrix.translate(deltaX, deltaY);

    // Apply the transformation matrix
    vectorRenderer->setTransformationMatrix(transformationMatrix);

    // Prepare command and coordinate arrays
    uint8_t cmds[MAX_POINTS] = {0};
    float coords[MAX_POINTS * 2] = {0};

    cmds[0] = VectorPrimitives::VECTOR_PRIM_MOVE; // First command is MoveTo
    coords[0] = points[0].x; // Initial x
    coords[1] = points[0].y; // Initial y

    for (int i = 1; i < numPoints; ++i)
    {
        cmds[i] = VectorPrimitives::VECTOR_PRIM_LINE; // Subsequent commands are LineTo
        coords[i * 2] = points[i].x;       // x-coordinate
        coords[i * 2 + 1] = points[i].y;   // y-coordinate
    }

    // Optionally, define a bounding box (not mandatory)
    float bbox[4] = {
    		absoluteRect.x, absoluteRect.y,
			absoluteRect.width, absoluteRect.height
    };

    // Draw the path
    vectorRenderer->drawPath(cmds, numPoints, coords, numPoints, bbox);
    vectorRenderer->tearDown();
}

 

 

Problem Description
The issue arises when:

  1. I scale the transformation matrix to ~1.7.
  2. I drag the drawn path halfway outside the visible window.

This results in an assertion error in the following code:

 

nema_buffer_t nema_buffer_create_pool(int pool, int size)
{
    nema_buffer_t bo;
    memset(&bo, 0, sizeof(bo));
    bo.base_virt = tsi_malloc_pool(pool, size);
    bo.base_phys = (uint32_t)bo.base_virt;
    bo.size      = size;
    bo.fd        = 0;
    assert(bo.base_virt != 0 && "Unable to allocate memory in nema_buffer_create_pool");

    return bo;
}

 

Question
When I set the bounding box for the drawing path, my assumption is that the Vector Renderer should not allocate memory exceeding the screen’s size. However, it appears that the assertion failure occurs because memory allocation fails (bo.base_virt == 0).

Does anyone know why the renderer might still attempt to allocate additional memory outside the defined bounding box, especially when the transformation matrix is scaled?

1 ACCEPTED SOLUTION

Accepted Solutions
TerZer
Associate III

For some reason setting scaled matrix to Vector Renderer gives that error:

vectorRenderer->setTransformationMatrix(transformationMatrix);

 So I just transformed points manually without setting Matrix to Vector Renderer:

Matrix3x3::Point point = transformationMatrix.affineTransform(points[i].x, points[i].y);

 And that fixed my issue with memory allocation.

View solution in original post

3 REPLIES 3
TerZer
Associate III

For some reason setting scaled matrix to Vector Renderer gives that error:

vectorRenderer->setTransformationMatrix(transformationMatrix);

 So I just transformed points manually without setting Matrix to Vector Renderer:

Matrix3x3::Point point = transformationMatrix.affineTransform(points[i].x, points[i].y);

 And that fixed my issue with memory allocation.

amb
Senior

Hello @TerZer 

    Can I ask how this code works? I have been looking for ways to draw lines more freely.

thanks.

TerZer
Associate III

Hello @amb ,
This code has comments. If you want to know what functions VectorRenderer has and why I called them you can check this documentation: https://support.touchgfx.com/docs/api/classes/classtouchgfx_1_1_vector_renderer