STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! TouchGFX Project using the H757i-EVAL Board

Hi, I decided to learn how to create GUIs using TouchGFX and upon creating a project on TouchGFX, 2 questions popped up on my mind:1 - There's no template for the H757i-Eval Board; what would be the right procedure? Is there still some sort of templa...

nnoK by Associate
  • 2317 Views
  • 3 replies
  • 0 kudos

Weird behavior when adding a new section to QSPI

Hello,I have a problem adding a new section to QSPI with the graphics stored on it.I want to store some error-text tables in a new section of the QSPI flash.For that i shrinked the 64MB QSPI and added a new section in the linker script. QUADSPI (r) ...

TouchGFX shows flicker on content update

Hiwe had made a custom STM32 board and we had some issues setting up TouchGFX. Display parallel interface with 800 x 480 pixels Model - > AT070TN94MCU: STM32H7B0VBT6External Flash QuadSpi W25Q128JVI use external Flash Boot LoaderLDTC Clock 32MHzThe i...

Resolved! MoveAnimator - Best practice to move an object

Hi,I'd like to discuss the best practice or approach to execute an infinite animation, like a GIF, to execute is while the screen is running.I've done a simple Box object, as an example purpose of my subject, to help in this topic. It could be line, ...

uilter by Senior
  • 4430 Views
  • 3 replies
  • 1 kudos

Resolved! Reply to post won't appear

I understand the forum has a brand new system now and there can be bugs. But why can't see my reply posts anymore?I posted a reply on my post but it won't appear. I tried it 5x already and even closed browser.