STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! How to create a custom triangular progress bar?

Hi I'm working since a couple of days with TouchGFX and a custom SPI-Display.Until here everything works fine. Even togheter with an RTOS.Now I would like to customize some sliders, progress bars and Icons.For me the most important question is, how t...

UZbin.1 by Associate II
  • 3301 Views
  • 5 replies
  • 0 kudos

STM32H745 on 16 depth

Hello, i have stm32h745i for my project but unfortunately the SDRAM itself is not enough to handle my gui program.I use lvgl and squareline studio to make gui. I have thought that maybe if i can reduce the color depth from 32 to 16 will reduce my mem...

BAl K.1 by Associate III
  • 2513 Views
  • 3 replies
  • 0 kudos

Resolved! TouchGFX Roadmap

Hello,I checked but I didn't find any information, is there a TouchGFX roadmap available somewhere ?Regard,NME

nme by Associate II
  • 4108 Views
  • 7 replies
  • 3 kudos

Touch GFX drawing a pixel.

HiWe are in the need to dynamically graph a moving point based on an analog input.We have a solution when using a regular display driver like RA8875, however our desire is to use Touch GFX as the solution includes more than 1 simple screen.Is there s...

Resolved! TouchGFX Code generating and Simulator error

Dear Mr MartinIn touchGFX I can generate the code but I can´t simulate with this error:Compiling generated/gui_generated/src/screen_screen/screenViewBase.cppgui/src/model/Model.cpp:4:10: fatal error: stm32f4XX_hal.h: No such file or directory#include...

Resolved! Communication from screen to backend

Hi,I'm trying to send an event when a button is clicked.I have added an interaction in Touchgfx designer to call a virtual function when the button is clicked.In Screen1view.cpp I'm overwriting the virtual functionvoid SendDataOnButtonClicked(){prese...

KNara.2 by Associate III
  • 2644 Views
  • 2 replies
  • 2 kudos