STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

STM32F746G-DISCO does not work with TouchGfx 4.22.1

Hello,I just bought a STM32F746G-DISCO from Mouser (Mouser #:511-STM32F746G-DISCO).When it arrived, the LCD and touchscreen were working well. However, after I downloaded the demo project (STM32F746G-DISCO Control LED from GUI v3.0.6) in the TouchGfx...

hbZhao by Associate III
  • 3928 Views
  • 4 replies
  • 0 kudos

Resolved! Thermostat with Touchgfx

Good Afternoon all, It could be possible to make a thermostat touch sensitive using touchgfx? Like that ones with temperature value in the center and a "slider circle around". Thanks in advance. 

Berto by Associate III
  • 3039 Views
  • 4 replies
  • 3 kudos

TouchGFX Performace Degradation in Landscape

I am using touchgfx 4.20.0 and have a project running well in portrait on a 2.4" tft screen (RGB565).My issue iswhen i rotate the project to be landscape some features become very laggy. for example i have a rotary dial and turning it up and down mov...

Resolved! make[3]: *** No rule to make target 'CM7/TouchGFX/build/Riverdi_70STM32H7/Drivers/STM32H7xx_HAL_Dri

Hello,I have a Riverdi screen with an embedded stm32H7. When I am trying to flash with the st-link the code to the screen I am getting this error. I need to mention that I didn't got this error before and the Makefile is auto generated. Could anyone ...

Resolved! Texts with multiple typographies

We have a design with a menu implementation that uses texts in multiple places with potentially different typographies (the translated text is used for menu entries, headings or keyboard edit screens). Example: We have a parameter "Modbus Address" wh...

SWT-GAL by Associate II
  • 1559 Views
  • 1 replies
  • 1 kudos