STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

linker error after upgrading to touchGFX 4.21.4

I have a full working project targeted to touchGFX 4.20 (compile and run fine). I've tried to upgrade to 4.21.4 but I have the following linker error:"Error: L6216E: Cannot use base/limit symbols for non-contiguous section .ARM.exidx"The migrating pr...

CDavi.3 by Associate II
  • 4061 Views
  • 6 replies
  • 0 kudos

Turn off drag for scrollable container

When I using handleDragEvent(const DragEvent& evt) function my application start to lagging. How to do that handleDragEvent function be called only when I touch image and not scrollable container? Draggable is turned off on scrollable container

heyo by Senior
  • 1430 Views
  • 1 replies
  • 0 kudos

Touch simulation

Is it possible to simulate touch? For example I touch one time but executes two touches on same XY? I have one hided image and then I touch list element that image appears and I need to drag it.

heyo by Senior
  • 1692 Views
  • 1 replies
  • 0 kudos

Resolved! Screen Transition on timeout

I am using TouchGFX and currently using simulator only. I want to change the 1st Screen after 2 Seconds. How can i achieve this timeout to change the screen. I explored all the widgets in the TouchGFX but i didn't get any option. Anyone has solution ...

SS.Sagar by Associate III
  • 3733 Views
  • 3 replies
  • 0 kudos

"The current target does not support vector font format"

I get this message in TouchGFX Designer when I try to change the font format to vector. This is the new advertised feature of TouchGFX 4.23.0. I have "Vector Rendering" and "Vector Font Rendering" enabled in IOC. What else is needed to enable vector ...

HTD by Senior III
  • 3277 Views
  • 2 replies
  • 1 kudos