STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

STM32U5A9J-DK IDE Problem

Hello everyone, when I compile the code with the designer and throw it away, there is no problem, but when I create it via CubeMX and open it in CubeIDE and compile it, I encounter problems.For example:STM32U5A9NJHXQ_FLASH.ld ->EXT_FLASH (r) : ORIGIN...

buyildir by Associate
  • 1072 Views
  • 1 replies
  • 0 kudos

Resolved! Clearing Dynamic Graph Data

Hello, I'm having issues trying to clear the data set from a dynamic graph in Touch GFX. Unfortunately none of the data points nor graph line are being cleared from the graph.The graph is set to scroll as more data is added. When a "user session" is ...

Resolved! Avoid Custom Code Deletion In TouchGFX

I'm am having trouble figuring out a good flow for using Designer and CUBE IDE to design a GUI. I am mostly using Designer (4.22) to draw graphics but can't seem to retain custom code when Designer generates code. For example, I am using the F769I-DI...

sergiog by Associate
  • 2432 Views
  • 3 replies
  • 0 kudos

Resolved! TouchGFX装完能打开,创建工程时,基本上到88%左右就卡住,然后就自己退出了,是什么原因?

这个问题是从4.22版本开始出现的,之前的4.20可以正常用,装完4.22后,出现这个问题,然后4.20版本也一样问题不能用了,我全卸载,装了4.23,这个问题依然存在,可能是什么原因,怎么解决? 

sipower by Associate II
  • 3256 Views
  • 3 replies
  • 1 kudos

DMA2D and LTDC double buffering

Hi everybody,I'm developing a simple gui on an STM32F429 microcontroller with the use of the STemWin grapich library. Everything is working well till I'm using just one framebuffer; now I would like to use double buffering to optimize the interface a...

andrea.l by Associate
  • 5709 Views
  • 5 replies
  • 1 kudos

Resolved! code not executing

sir we are generated code through touchgfx(stm32f508-dk) , the display part working good as per our requirement ,but when add led toggle code in while condition in that code ,its not working , before while condition we added led on and off for 10 sec...

kishor by Associate II
  • 6462 Views
  • 6 replies
  • 0 kudos