2023-06-29 6:01 AM
Dear Mr Martin
In touchGFX I can generate the code but I can´t simulate with this error:
Compiling generated/gui_generated/src/screen_screen/screenViewBase.cpp
gui/src/model/Model.cpp:4:10: fatal error: stm32f4XX_hal.h: No such file or directory
#include "stm32f4XX_hal.h"//obrigado declarar
^~~~~~~~~~~~~~~~~
compilation terminated.
I already reinstall TouchGFX, I already rebuilt all my project in STM32CUBEIDE and nothing.
This library is present in the Stm32cubeIDE path project.
Do you have any idea of what is causing this error: thanks, Best regards.
PS:TouchGFX 4.22.0-STM32F429
Solved! Go to Solution.
2023-07-06 10:28 AM - edited 2023-07-06 10:30 AM
Hello
Still cannot see the East sliding transition between screens if 'none' is selected. I import your GUI to empty F769i-DK template, so I could run it also in target.
For moving textareas I would do something like this, it seems to work OK:
textArea1_1.invalidate();
textArea1_1.setPosition(119, current_bargraph_value, 80, 46);
textArea1_1.invalidate();
So just in case invalidate it before and after moving. Then also add
textArea1.resizeToCurrentText();
After the changing the textarea content, it looks nice then horizontally also.
In attached project there is used 'moveTo' function for other text area (textArea1).
I make to model.cpp simple sender to send different values and bar sizes.
You can test it if you want, just open touchgfx file, you can run it on simulator. It only simulates the bar/text area changes, just set the switch on :thumbs_up:. All target specific stuff is #ifndef away since there wasnt .ioc file in your packet.
Due the 3 x 5MB limitation here the target (F769DK) dont work, only simulator.
2023-07-01 5:11 AM - edited 2023-07-01 5:12 AM
Hello
Im not Martin but lets try :D
Sounds that you must use #ifndef directive to remove that like this in model.cpp:
#include <gui/model/Model.hpp>
#include <gui/model/ModelListener.hpp>
#ifndef SIMULATOR
#include "stm32f4XX_hal.h"
#endif
You might need to remove same way also all other target-specific .c/.h externed code in model.cpp.
You can also use this other way around, for example to generate some test calls from model.cpp to presenter when running simulator
void Model::tick()
{
#ifdef SIMULATOR
tickCounter++;
if(tickCounter>=60) // 1 sec ?
{
tickCounter=0;
modelListener->doSomething(someValue);
}
#endif
}
2023-07-04 5:14 AM
Hi Mr.JTP1
Could you please tell me how can I report bugs in Touchgfx 4.22.0?
I´m having more problems in my project (stm32f429 Touchgfx4.22.0 stm32cubeIDE 1.12.1 ) than effectives results.
I´m not doing simple applications, like change color of the screen or blink led and so on.......).
For example, when I chose "NONE" transition in interaction change screen the result is a slider East transition.
When I change the text area position the result is clipping characters in the display.
well.....Another question:Where I can find documentations about flex button?
Which are the equivament command for getState and forceState for FLEXBUTTON?
THANKS A LOT, BEST REGARDS
2023-07-04 5:35 AM
Dear Mr.JTP1
This proposal solution :
#include <gui/model/Model.hpp>
#include <gui/model/ModelListener.hpp>
#ifndef SIMULATOR
#include "stm32f4XX_hal.h"
#endifDidn´t make any effect in the Touchgfx error messages.
Could you please think in another one? thanks
2023-07-04 9:48 AM
Hello
Some comments on green:
@fpgiovanini wrote:Hi Mr.JTP1
Could you please tell me how can I report bugs in Touchgfx 4.22.0?
One (and maybe only) way is to report bugs here with clear instructions how to reproduce it. Maybe even small example project helps if its difficult to repeat.
I´m having more problems in my project (stm32f429 Touchgfx4.22.0 stm32cubeIDE 1.12.1 ) than effectives results.
I´m not doing simple applications, like change color of the screen or blink led and so on.......).
For example, when I chose "NONE" transition in interaction change screen the result is a slider East transition.
Weird, with quick test it seems to work in 4.22.0 OK. Can you share your project or TGFX part from it ?
When I change the text area position the result is clipping characters in the display.
How do you change the text area position ? I guess best way is to use MoveTo command, then its not needed to invalidate anything.
well.....Another question:Where I can find documentations about flex button?
https://support.touchgfx.com/docs/development/ui-development/ui-components/buttons/flex-button
Which are the equivament command for getState and forceState for FLEXBUTTON?
You can use getPressed and setPressed to read and set the state.
If you set trigger as toggle, you can use also forceState.
2023-07-06 5:27 AM
Hi Mr.JTP1
Weird, with quick test it seems to work in 4.22.0 OK. Can you share your project or TGFX part from it ?
Attached!
How do you change the text area position ? I guess best way is to use MoveTo command, then its not needed to invalidate anything.
Besides moving the textarea Position I need to update the value and the "line" widget on line.(see the application please).
Unicode::snprintfFloat(textArea1Buffer, TEXTAREA1_SIZE, "%02.2f", voltage_finalData);
textArea1.invalidate();
2023-07-06 10:28 AM - edited 2023-07-06 10:30 AM
Hello
Still cannot see the East sliding transition between screens if 'none' is selected. I import your GUI to empty F769i-DK template, so I could run it also in target.
For moving textareas I would do something like this, it seems to work OK:
textArea1_1.invalidate();
textArea1_1.setPosition(119, current_bargraph_value, 80, 46);
textArea1_1.invalidate();
So just in case invalidate it before and after moving. Then also add
textArea1.resizeToCurrentText();
After the changing the textarea content, it looks nice then horizontally also.
In attached project there is used 'moveTo' function for other text area (textArea1).
I make to model.cpp simple sender to send different values and bar sizes.
You can test it if you want, just open touchgfx file, you can run it on simulator. It only simulates the bar/text area changes, just set the switch on :thumbs_up:. All target specific stuff is #ifndef away since there wasnt .ioc file in your packet.
Due the 3 x 5MB limitation here the target (F769DK) dont work, only simulator.
2023-07-07 7:36 AM
Dear Mr.JTP1
IT REALLY SOLVE THE PROBLEM!!!THANKS