STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! TouchGFX on H7A3ZIQ 230x 'undefined reference'

Hi,I have used TouchGFX on an F4 without any problems so far, except that the animations were a bit slow. Now I bought this H7A3ZIQ and when I add TouchGFX to the project, I get 230 'undefined reference' errors. Any ideas on how this is possible?

wtf_h7.jpg
kr36 by Associate
  • 2537 Views
  • 3 replies
  • 2 kudos

Resolved! Remove unused functions

Hello,I am working on H750 while the flash is limited.Because the LCD is RGB565, may I know if the the unrelated functions can be removed? such as functions related with ARGB8888 and RGB888.  Thanks.   

hbZhao_0-1720819584764.png
hbZhao by Associate III
  • 5243 Views
  • 6 replies
  • 0 kudos

Video decoding for STM32H7B3L.

Hi.I am using SDRAM, OctoSPI and 24bit RGB888 TFT screen. Project is working normally with another widgets (button, shape, text area, image etc.). Now i want to use video decoding and video widget. I made the necessary cubemx settings by reading the ...

DMA2D.png jpeg.png jpeg1.png jpeg2.png
ABURM by Senior
  • 7879 Views
  • 14 replies
  • 0 kudos

Resolved! Touchgfx simulation error

Hello everyone,I recently downloaded TouchGFX version 4.23.2 and tried running the example on my STM32F7508-DK. However, when I click the simulation button, I encounter these errors. Can anyone help me with this issue? I'm running TouchGFX on Windows...

rohamid by Associate II
  • 7954 Views
  • 11 replies
  • 1 kudos

STM32H745, Use of TouchGFX, Ethernet and LwIP

I am currently working on a project using TouchGFX, Ethernet an LwIP on a STM32H745I board and I was wondering if anyone has encountered a similar issue.I am using :the firmware package v1.9 for the H7 (I also tried with the v1.10),TouchGFX 4.18 (I a...

0693W00000QKwdtQAD.png
QRobe.1 by Associate II
  • 3489 Views
  • 5 replies
  • 2 kudos

Resolved! TouchGFX 4.24.0 new project creation error

I simply wanted to create a new TouchGFX project for Riverdi STM32 Embedded Display.  It gave me "Combination of Riverdi STM32 Embedded Display & Blank UI failed" error all the time.I've tried uninstall the legacy versions and re-install, but no luck...

Screenshot 2024-07-04 104133.png Screenshot 2024-07-04 113909.png Screenshot 2024-07-05 094245.png
Eric Z. by Associate II
  • 5873 Views
  • 8 replies
  • 4 kudos