STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Slide controls implementation

Hi,if I understand correctly, TouchGFX does not support sliders. What is the simplest and safest way to implement them for a newbie to the ST ecosystem and tools?More specifically two types: scrollbars (of a text window) and date-picker wheel.As a si...

Ricko by Senior III
  • 1863 Views
  • 3 replies
  • 3 kudos

Resolved! Add name of container for items in screen

It would be useful if an item (widget) added to a screen which is a container, showed the name of the container in the properties window. I have a lot of different containers and if I need to make changes to the container, sometimes I have to go thro...

GMeta.1 by Associate III
  • 1416 Views
  • 2 replies
  • 0 kudos

Resolved! using TouchGFX with only internal ram

Hello, I'm developing using stm32f476-DISCO. Until now, we have made development easy by using external RAM. The current operation has received a request to create a program using only internal RAM without external RAM.   https://support.touchgfx.com...

JIN3473 by Associate III
  • 1722 Views
  • 1 replies
  • 0 kudos

simulator lauch bad application !

hi I have a problem, when I launch the simulator it does not launch the right project. My project is GP_Dash_70_V1_a not MyApplication_10.MyApplication_10 is a project that I deleted a long time ago.I do not know what manipulation I could have done t...

Capture.PNG
NicoEFI by Associate III
  • 2141 Views
  • 4 replies
  • 0 kudos

TouchGFX library

I installedTouchGFX Designer and want to add components to my project but there are only a few in the provided library. I even did not find the buttonUp that was used in the Button Example. Where can I get more components ? I want to make 3D vector f...