STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

TouchGFX error

I'm using STM32F423ZHT6 board.I setup the X-CUBE-TOUCHGFXAnd FSMC for LCD interface:After generate a code. I opened TouchGFX -> ApplicationTemplate.touchgfx.part.In TouchGFX, I created a boxWithBorder Then Generate code. After Build my project, It sh...

Meenakshi_0-1724842209722.png Meenakshi_1-1724842302363.png Meenakshi_2-1724842540032.png Meenakshi_3-1724842624701.png
Meenakshi by Associate III
  • 1897 Views
  • 5 replies
  • 1 kudos

Resolved! TouchGFX designer, CubeMX generation order?

Hello all,I'll be starting a project in TouchGFX designer from an existing template, say STM32F469I DISCO. How does the code generation by the TouchGFX designer and CubeMX interact? Say when I add an UI element and regenerate the code in designer, do...

Martin294 by Associate III
  • 2220 Views
  • 4 replies
  • 0 kudos

Rename project for opening in STM32CubeIDE

Hello all,I am trying out different projects based on the F469I discovery board. Unfortunately they show up in STM32CubeIDE as having the same name, so it refused to open them.This problem has been around for a long time, with a rather ugly workaroun...

Martin294_0-1723908818806.png
Martin294 by Associate III
  • 2882 Views
  • 5 replies
  • 0 kudos

Access line widget from own source file

Hello, I am trying to modify the start and end points of a line I have created in TouchGFX from outside of the screen code generated by touchGFX.  I would like to be able to modify the end points from my own source code files by calling line1.setEnd(...

brohr01 by Associate III
  • 671 Views
  • 1 replies
  • 0 kudos