STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! RGB image compression memory fault

Hey,I am trying out the new RGB image compression in TGFX 4.24 and are having some issues. My program compiles fine without any compression.I have only turned the feature on in TouchGFX Designer and generated code. Is there something else I am missin...

PontusL by Associate III
  • 3803 Views
  • 7 replies
  • 0 kudos

Resolved! touchgfx scrollWheel callback not working

 I cannot get scrollWheelUpdateItem callback to fire when the scrollWheel is moved. void Button1MenuView::scrollWheelUpdateItem(MenuElement& item, int16_t itemIndex) { // Override and implement this function in Button1Menu item.setNumber(itemInd...

FJB2069 by Senior
  • 1028 Views
  • 1 replies
  • 0 kudos

Resolved! Freertos Event link error

I started to getting this error from touchgfx after I added an Event throught CubeMX. As you can see from the messages, this is exactly what the errors are about.Compiling Core/Src/main.cLinking TouchGFX/build/bin/target.elfTouchGFX/build/STM32F429ID...

Wiser1201 by Associate II
  • 1102 Views
  • 1 replies
  • 0 kudos

Resolved! Hardware video decoding problem.

Hi guys.I've been trying to work hardware video decoding for a few days but it doesn't work. Latest situation is as follows:I think I made all the settings correctly.1- Enable JPEG.2- Enable MDMA channel 6 and 7 for JPEG output fifo - input fifo.3- E...

ABURM by Senior
  • 3589 Views
  • 3 replies
  • 1 kudos