STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! TouchGFX Designer - Program and Run Target Failed

I am using TouchGFX Designer standalone and can build and simulate my project ok, but Program and Run Target fails with 'recipe for target '_extflash_' failed' even though STM32CubeProgrammer is connected to the STM32F7508-DK  board that I am using. ...

250113 TouchGFX Program Error.png
alw by Senior
  • 1793 Views
  • 2 replies
  • 2 kudos

Resolved! TouchGFX code optimization - unused code?

Originally a reply here (solved), but split to a separate thread as it is a new question.Hello,Is there any  way to disable the code which is auto generated by the Touch GFX  designer which is not used by the application. so I can reduce the space of...

Resolved! How to rotate the image in TouchGFX?

Hi there,In my STM32F429BI TouchGFX project, I using some images.I want to show a image in areaA, and then rotate the image 90dgr and show it in areaB.But seems I must store the 2 images(before and after the rotation) in RAM to show both of them.Can ...

Junde by Senior III
  • 2570 Views
  • 3 replies
  • 1 kudos

X-CUBE-TOUCHGFX 4.24.2 is out!

TouchGFX 4.24.2 is now out. Please follow this link to download it.Release details: Release date: December 18th, 2023 New TouchGFX Core Features: Added libraries for cortex M55.We're happy to share a new TBS in the TouchGFX Designer based on this co...

OsmanSOYKURT_0-1734955106312.png

touchgfx breaks ethernet connection

hello,I customized a board with stm32h743iit6 for HMI application, the main hardware features available on the board are RMII ethernet, 32bit SDRAM and LTDC RGB565 interface. Below is the board picture.A test MDK keil project is generated by cubemx t...

微信图片_20250104114456.jpg wonderFine_0-1735963299350.png wonderFine_2-1735965166074.png