STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1823 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4967 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9725 Views
  • 5 replies
  • 3 kudos

Resolved! Motor Control Board Customization

Hi every oneI have defined a custom motor and inverter successfully.Now I need to define custom features like a simple Digital output(LED for instance).Is there any way?or should I cut working on stmcubemx and continue coding after code generated by ...

Carador by Associate II
  • 3422 Views
  • 8 replies
  • 0 kudos

Resolved! FOC Open Loop API

Hello Everybody,MCSDK:6.3.0CubeMX: 6.3.0Workbench : 6.3.0Motor Pilot : 1.2.9I used open-loop voltage on the motor pilot to perform tuning with (voltage_ref, TargetSpd) at the following settings: (10%, 300), (20%, 600), and (30%, 900), each with a dur...

Vincent7 by Associate III
  • 2298 Views
  • 2 replies
  • 1 kudos

Resolved! Force PWM signals to lock the rotor in fixed position

Hi, I am using the P-NUCLEO-IHM03 STM32 motor-control pack along with a AMS AS5147U rotary sensor for speed control with Hall-effect. The rotary sensor needs to be calibrated by setting a zero angle aligment. This is done by disconnecting the motor f...

roar by Associate II
  • 2428 Views
  • 2 replies
  • 2 kudos

Resolved! STM32G030C8Tx can not communicate with BTT TMC2209

I have STM32G030C8Tx C project that I am trying communicate with BigTreeTech TMC2209 module with the UART half duplex interface. I have attempt to write the code from scratch, kicked that around for a few weeks, gave up and tried to port over some ar...

Screenshot 2025-01-09 133933.png Screenshot 2025-01-09 135856.png
Moonless by Associate
  • 2121 Views
  • 2 replies
  • 1 kudos

Resolved! MCSDK 6.3.2 and STM32H753

Hello everyone,I have an existing project on the STM32H753VIT6 and I need to add three-phase motor control (FOC mode) via STDRIVE101 driver. The question is whether my approach to importing the MCSDK into my project is correct.Due there is no support...

error_1.png
AndriiD by Associate
  • 1252 Views
  • 1 replies
  • 0 kudos

B-G431-ESC1 Board: ST890 issue

As my understanding, ST890 used for isolate USB 5V and Battery 5V( DC/DC from 10V by U12: LDFPVR ). And also provide 5V for ESC board in debug program even  without battery connected.But why when I use battery only, which means no usb pluged, there i...

Kai123_0-1736517262389.png
Kai123 by Associate
  • 705 Views
  • 0 replies
  • 0 kudos

How to use nucleo-IHM08M1 on nucleo stm32f767

Hey I was I wondering if it was possible to use the x-nucleo-ihm08m1 on an 144 board.I only have 144 pin boards but couldnt find my board on MC Workbench.I also tried the motor pilot software and it said to configure the board.I suppose I can use it ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.