STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1742 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4891 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9592 Views
  • 5 replies
  • 3 kudos

Could someone help with MCP overrun errors ?

Hi, first the good news: I have motor control up and working. And communication with the workbench works fine. Having read up on the ST motor control protocol, and watching serial comms with the HHD software device monitor app, I can see that command...

DKing.1 by Associate II
  • 1697 Views
  • 2 replies
  • 0 kudos

how to connect the interface timer to the PWM generating timer using DMA on a STM32G4 for BLDC motor coordination using three (U-V-W) Hall Sensors?

I want to use an STM32G4 to control a BLDC motor with three (U-V-W) Hall Sensors (through a TI DRV8323S three-phase integrated gate driver). To be concrete, I am planning on using TIM1 on the STM as the interfacing timer to detect state changes (on U...

TB by Associate III
  • 1609 Views
  • 1 replies
  • 1 kudos

Six-step motor driving library for STSPIN32F0251

Hi All,Please has anyone worked the six step library STSPIN32F0251 for the EVSPIN32F0251S1 evaluation board ?if yes, please do you mind explaining this: When the quasi-synchronous rectification is selected under the 6step_conf.h file, the MC_Core_LL_...

0693W000008xaPWQAY.png

I am using STM32F405 for BLDC six step motor control for drone application with open source BLDC VESC code. In the PWM pulses for the low side IGBT’s, there is a weird pulse (which is unwanted) and causing problem especially during high duty cycle

The captured PWM signals with back-emf’s and currents are shown in the figure below (waveforms are recorded using Logic Analyzer). The pulse causing the problem is highlighted in yellow.I did many work-around to solve the problem but could not find a...

0693W000008xoeQQAQ.png
JJaco.3 by Associate
  • 1188 Views
  • 1 replies
  • 0 kudos

Flash programming while MC Workbench program is running

Hi, I'm going to write a parameter tabe into the last page of the flash in my MC Workbench project running on STM32F302R8. I made some tests and seems that programming the flash while the motor is in IDLE state is working fine. If I program the flash...

CSime.1 by Associate
  • 857 Views
  • 1 replies
  • 0 kudos

Generated Project is showing IPConfigManager:1461 error.

I am geeting errors when generating the project for EVSPIN32F0601S3, this concludes with: Completed with Errors.So, when I close the Project Generation, the Workbentch says Generation failed.I have now changed the location where the projects are bein...

SBung.1 by Associate II
  • 1254 Views
  • 2 replies
  • 0 kudos

STM32F4 Discovery Board external power problem

Hi,I am trying to feed my Stm32F4 Discovery with 5v in pins. I have tried to feed it with ESC's BECs , PDB or with voltage regulator and Li-Po battery but I am still facing with problems.The problem is that when I try to make PWM generation in tim4 ...

MDoğr.1 by Associate II
  • 1118 Views
  • 1 replies
  • 0 kudos

How can change the RPM using motor control SDK API.

Hi, SETUP:IPM30B-3sh + STM32F302R8 + 2.5KW BLDC MotorI have been trying to run the motor sensorless + PLL, i have been able to run the motor with predefined ramp.question:Q1. How can control the speed of motor using the gui tool and knob in MC-Workbe...

Tido1 by Associate
  • 1065 Views
  • 1 replies
  • 0 kudos

How is motor power computed in MC Workbench projects?

Hi, I developed a project for a 1Hp PMSM motor with FOC algorithm. Expecially when running at low speed motor power given by MPM_GetAvrgElMotorPowerW() function is about 20% more than the real power. Hand computation based on RPM, Ke, Iuvw gives inst...

CSime.1 by Associate
  • 991 Views
  • 1 replies
  • 0 kudos