User Activity

I am using the NUCLEO-G474RE along with the X-NUCLEO-SRC1M1 board to create a USB-C power delivery source. I am also using the "SRC1M1_Source" example project in the x-cube-tcpp software download.I am attempting to provide a 20V, 5000mA source to a U...
When I try to start my motor by programming a torque ramp and starting the motor, if the motor fails to start, the motor state moves to FAULT_NOW with a startup error. The real issue is that I don’t know how to clear the fault. The state never change...
I am working working with a PMSM FOC project in MC Workbench 6.2.1 and I am wondering if there is a way to change the mcu's analog vref input voltage. From the numbers I'm seeing on the current measurement page, it seems like MC Workbench is expectin...
I am trying to launch a MC Workbench project targeting a STM32G431CBUx mcu as the controller. I tried to modify an existing control board file to use the STM32G431CBUx as the mcu. I am able to select my custom control board on the selection page, as ...
Kudos given to