User Activity

Hi I have a question.I wanna get to multiple value using RCM Function. main.c It's not working.(Debug mode) I see everything working fine in my previous application where I used only one ADC channel and one RCM registration.Why multiple is not workin...
Hi I have a question.I wanna get to multiple value using RCM Function.  main.cLive expression I see everything working fine in my previous application where I used only one ADC channel and one RCM registration.Why multiple is not working?
I am planning to drive the motor with FOC using the EVSPIN32G4 board.MC_WorkBench 6.3.0ST Motor Pilot V1.2.0 - profilerI checked the motor parameters with the ST Motor Pilot V1.2.0 - profiler program.And I created a project with the EVSPIN32G4 board ...
I found the motor value using the Motor Profiler 5.4.8 program (P-NUCLEO-IHM002).(Figure1)The Motor Pilot_6.3.0 program does not connect using UART.(Discover Board / Launch Profiler)(Figure3)Even if I change the UART Speed, the "Port Open and try to ...
I used the Motor Profiler 5.4.8 program to extract the motor values ​​of the 12v custom motor in picture 1 and created a project in MC_Workbench to operate it. I bought an evspin32g4 board to test the operation of a larger voltage motor.How can I ext...