User Activity

I am using B-G431B-ESC1 board and GBM2804H-100T Brushless Gimbal Motor, properly generated the code. But upon receiving PWM signal, Motor is behaving:Motor spins then zero spins then zero soon then spins.Although Motor is working with other controlle...
I am using STEVAL-ESC001v1 and a2212/10t 1400kv motor. While giving it supply and reference signal, the measured speed keep on increasing and the actual speed of motor as well. Also, motor_state stucked at START but motor still running. Please help. 
I am using STEVAL ESC 001V1 and enabled Field weakening with FOC, but motor is not running, it is starting, stopped, starting stopped and soon. I also seperately tried setting Id = -ve value but its not working. Please help.
 I am trying to understand SVPWM logic developed by ST, from mc workbench, i referred the documentation provided. But its much unclear in the documentation as well why and what variables are being used for. I want to know the reference of the literat...
For steval esc001v1 with MC workbench Version: 6.3.0, to run firmware do we need any other connections other than below mentioned because motor is not running?Connection: 12V DC input SWD connections with STLink3 phase motor wire connection at OUT1,2...