STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1746 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4897 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9604 Views
  • 5 replies
  • 3 kudos

Overload Derating

I want to know the overload based derating, there will be continuous current and the peak current. If the current exceeds continuous current for a certain duration i consider overload. What to be done i do not know. Does ST has any application notes?

JDesi.1 by Associate II
  • 1202 Views
  • 1 replies
  • 0 kudos

STEVAL IHM034V2 evaluation board, three phase induction motor is not running, PWN and IPM module is not working

Hi,i'm using the a STEVAL-IHM034V2 board for evaluation (PFC + FOC PMSM).i am using three phase induction motorwell I am using the Motor Control Workbench 5.4.7, for generating code , Keil uVision5 for burring the code in Controller ,  the code is bu...

MAhme.5 by Associate
  • 2251 Views
  • 1 replies
  • 0 kudos
GSeme.1 by Associate II
  • 2094 Views
  • 2 replies
  • 0 kudos

How I connect to Steval-IPM15B ?

I have Nucleo-F302R8T6 and STEVAL-IPM15B. But I don't know how to connect the pins. I tried to connect it by looking at the pins from the Motor control workbench program, but some pins were exposed, RX, TX pins were exposed. Can you help me how to c...

Eakso.1 by Associate II
  • 1979 Views
  • 2 replies
  • 0 kudos

Weired output then OC, and controller damaged

Hi all,​I am using f303rb with ihm08-1sh to control a motor, motor control is MCSDK 5.3.2Using HSI which has 64MHz clock speed.I set the PWM frequency to 15K, and FOC execution rate = 2.In most time, it works okay.In a very low probability, it will O...

0693W00000HpcxzQAB.bmp
JHSU.16 by Associate
  • 1635 Views
  • 2 replies
  • 0 kudos

Fanuc motor locked when I start the controller

Hello everyone!I'm developing an application with a little Fanuc Beta Series motor with a custom encoder. I was using a NUCLEO-F446RE, but it burns some tests ago :( Now I'm using a Chinese board with an F103C8T6, but not working properly.I attached ...

VFerr.2 by Associate II
  • 3198 Views
  • 3 replies
  • 0 kudos

ESD protection diode in powerSTEP01

In the powerSTEP01 datasheet, it is mentioned that VSREG must be always less than VBOOT (and VCCREG must be always less than VCC) in order to avoid related ESD protection diode turn on. The device can be protected from this event by adding an externa...

0693W00000GYZwCQAX.png