B.4
Associate II
since
2021-03-28
2023-06-14
User statistics
5
Posts
0
Solutions
0
Kudos given
0
Kudos received
STMicroelectronics Community
About B.4
Options
Report User
User Activity
Posts
Replies
how to connect steval IPM10B and nucleoL476RG board connection
2023-05-11
Avoid back emf on steval-spin3201
2021-11-11
Back emf from the motor is entering into other digital causing some issues. How can i avoid/isolate this back emf on STEVAL-spin3201
I am using steval-spin3201 board, Speed control loop running at FOC frequency of 13kHz.Quadrature encoder is used as feedback sensor.Motor works most of the time, but sometimes it starts running at max RPM in reverse direction. Please help
2021-03-29
Re: MCSDK 5.4.3/5.4.4. FOC ,Sometimes after encoder alignment ,motor run reverse。
2021-03-30
Hi @ypu ,I want to try second way, please explain configuration and Connection (like main & auxiliary) of the sensors.
Re: MCSDK 5.4.3/5.4.4. Sometimes after encoder alignment ,motor run reverse。
2021-03-28
Facing the same issue. I am using spin3201 running at FOC frequency of 13kHz.please help me out from this encoder alignment issue