STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1816 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4958 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9718 Views
  • 5 replies
  • 3 kudos

Resolved! How to demo EVSPIN32G4

Hello, I am a newcomer and want to ask a newbie questionI researched EVB-EVSPIN32G4 and found that there is no example of this.Both Demostrations need list EVB profile. So I can't directly operate them.1. ST Motor profiler2. MC WorkbenchWhat time doe...

Resolved! NEW STM32 MC-SDK version 5.Y.3

Dear STM32 Motor Control community membersWe are very pleased to announce the new release 5.Y.3 of the XCUBE_MCSDK. As usual, you can download XCUBE_MCSDK here: https://www.st.com/en/embedded-software/x-cube-mcsdk.html .The Motor Pilot, our monitorin...

How to up sample with non-integer clocks?

I have a motor control application where there is phase feedback at about 170Hz from a PID but this varies in application from 165Hz to 185Hz. The outer phase loop is summed with the inner speed loop (STM FOC Library) that has a crystal based 1kHz sa...

BTrem.1 by Senior II
  • 1089 Views
  • 1 replies
  • 0 kudos

I am using STEVAL-ESC001V1 for sensorless BLDC motor MN4006. I have downloaded IAR IDE Tool. But getting error in compiling. Error which i am getting i have attached with this email.

I am using STEVAL-ESC001V1 for sensorless BLDC motor MN4006. I have downloaded IAR IDE Tool.I have opened  STM32303C-EVALSINGLEDRIVE workspace in AR IDE. After compilation I am getting 3 errors which i have attached with this mail.Help to sort out th...

VSabn.1 by Associate II
  • 2008 Views
  • 2 replies
  • 0 kudos

Hall position / speed at low speed

Dear MC SDK team,We are experiencing oscillation at low speed in torque control with Hall sensors as main sensor. In the picture attached, motor is mechanically locked and Iq current reference is set to 3A. As you can see in the picture Hall angle is...

ANICO.1 by Associate III
  • 2486 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.