STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1717 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4869 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9546 Views
  • 5 replies
  • 3 kudos

A doubt with ICS topology

Hello everyone! It's a pleasure to participate of this forum.I developing a custom hardware with two ICS (Isolated Current Sensor) and i have a question. With this configuration MCSDK receive a sin wave signal, right? Just to clean up the doubt.Thank...

VFerr.2 by Associate II
  • 1150 Views
  • 1 replies
  • 0 kudos

Why have I "Error: Speed feedback" after run?

I use Schematic diagram of "EVSPIN32F0251S1" in my design with Hall Sensor and I use all its configuration for my board :and I used a below BLDC motor :power:300Wcurrent:10.5Avoltage :36Vspeed:3000 RPM but I do not have any move in my motor and outpu...

0693W00000GZUJCQA5.png 0693W00000GZUCkQAP.png 0693W00000GZUKoQAP.png 0693W00000GZURuQAP.png

Torque control with absolute encoder which outputs ADC.

I check to run motor with sensor-less FOC, and I referred to UM2374.​​I have the boards "Nucleo-F401RE" and "X-Nucleo-IHM08M1 3Sh".​so I need to control the constant torque even in case of motor stop.and I would use the absolute encoder type, it outp...

JPark.29 by Associate
  • 1156 Views
  • 1 replies
  • 0 kudos