STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1740 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4888 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9587 Views
  • 5 replies
  • 3 kudos

Resolved! meaning of "motorDrives" properties

For implementing our own hardware, I'm using the Board description of a B-G431B-ESC1 as a template.The "motorDrives" object declares some properties, like "maxRatedCurrent", "minRatedVoltage", "maxRatedVoltage" and "resistorOffset".None of those are ...

DMeie.2 by Senior II
  • 1319 Views
  • 1 replies
  • 2 kudos

steval_ESC002V1

I WAS BOUGHT STEVAL_ESC002V1 DEVELOPMENT  BOARD FROM ST. I DONT KNOW HOW TO USE IT.( HOW TO GIVE THE PWM INPUT VIA EXTERNAL).AND ALSO ITS NOT HAD ANY INYERNAL FIRMWARE. I AM ALREADY  DOWNLOAD  STSW FIRMWARE .ITS A BINARY FILE.HOW TO I LOADED & IS IT ...

6-Step on working on some boards

Hi, I am looking to try the 6 step commutation for a BLDC motor. I am using MC Workbench 6.2.0 however when selecting 6-Step, the EVALSTDRIVE601, and a nucleo G431, the BEMF sensing isn't detected and the BEMF feedback pins aren't listed in the pinou...

STM32 MotorControl Workbench Printf debug message

Hello STM32 Community,I am currently working with the STM32 MotorControl Workbench framework, specifically using the EVSPIN32G4 demo board. For development, I'm utilizing the STM32CubeMX and STM32CubeIDE tools.My issue lies with debugging. I'm attemp...

kaps by Associate II
  • 7499 Views
  • 10 replies
  • 1 kudos

Version Control & CI-CD with MC Workbench Project

Hi,I have done version control and CI-CD for large-scale C & C++ projects but I am not sure how to do this for the STM32-based tools and projects generated.For the Motor Control Firmware Development task I am currently assigned, I need to develop a s...

smaiti by Associate III
  • 1026 Views
  • 0 replies
  • 0 kudos

ACIM and NUCLEO-G431RB

Hello Everyone,  I'm trying to perform a command for ACIM, I created the code generated by MotorControl Workbench 6.2.1 without any problems and I'm using the NUCLEO-G431RB kit..I'm analyzing the PWM signals on the oscilloscope together with a filter...

Doubt.png
Gabe by Associate
  • 1279 Views
  • 0 replies
  • 0 kudos

B-G431-ESC hall voltage pin

Hi, I am using B-G431-ESC to control a brushless motor. Using Arduino and simpleFOC, I am able to control the motor in open loop setup. When tried using hall sensors pins, i see that there is no voltage on 5v pin on the esc board. The multimeter show...

STM.png STM2.png