User Activity

I have a hard fault on startup of my near clone of a B-G431B-ESC1 pcb.Generated the code using the latest version of MC (6.2.0). Code runs and waits for a start command from Motor Pilot. It then tries to start with a short burst of high current which...
Version of MCSDK 6.1.2Firmware,MC WB,DETAILSI have a B-G431-ESC1 board, and a custom board based upon that.Although using the STM32G431CBT6 chip, the major difference is really the current shunts being 0.2 mOhm. This together with total gain of 40.8 ...
I have a custom board based upon the B-G431B-ESC1. Using the LQFP48 foot print version of the same chip. It is missing a few pins, but my project is not using them.After creating a new project using STM32G431CBT6 and the importing the original from M...
Hello all,I have a 20 pole pair, 100v, 120Amp, 15mOhm. 34uH,  sensorless, BLDC outrunner motor.I have had this running on the B-G431B-ESC1 dev board with 25v at 800 RPM drawing 1.5 Amps. The power supply being lab bench supply capably of 30vDC and 5A...
Posted on June 29, 2016 at 15:11Hi there, I'm implementing a bootloader. And have created an application vector table that is different to the bootloader vector table Boot Vectors at 0x08000000 App Vectors  at 0x08010400 volatile const void (*vector...
Kudos from
Kudos given to