cancel
Showing results for 
Search instead for 
Did you mean: 

Motor profiler MCSDK 6.2.0

APerr.3
Associate II

I am moving to MCSDK 6.2.0 and want to test the motor profiler new feature. 

[VERSION]: MCSDK 6.2.0

[TOOL]: Motor PROFILER v1.2.4

EVALSTDRIVE101 + NUCLEO-F746ZG + Custom board for adapter

[DETAILS]: Fail to do motor profiling

[EXPECTED BEHAVIOR]:  Able to do motor profiling even with custom board

Attached is the project

 

The resistorOffset is not defined for the EVALSTDRIVE101, so I first do the offset detection. Measured value is approximatly the know motor resistor and resistor offset is therefore negative. 

Then I start profiling the motor but stay stuck with the message to increase (or decrease) the max speed. I have tried different value without success.

 

I know that this Power board is not listed in the table 2 (list of described boards containing resistorOffset parameter) in the motor profile page. And this board combo was not compatible with motor profiler in the past. But should I expect to work with MCSDK 6.2.0 ?

 

When I am injected the motor known information from my 6.1.2 project, it does not work straight out of the box. But for this point I need to investigate a bit more.

 



 

Thanks.

 

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Zied b.
ST Employee

Hi @APerr.3 
We will gradually add the Resistor Offset necessary to the Boards we support. For the EVALSTDRIVE101 board, I found a Resistor offset of 0.015, you can add

"resistorOffset": 0.015,

to the Board's .JSON file , Then start your profiling, normally you should have no problems.
Regards

If you agree with my answer, please accept it by clicking on "Accept as solution".
APerr.3
Associate II

Hi @Zied b. ,

 

Thanks for your response.

I managed to get the profiler working with another motor. The offset is still negative. And the motor is very noisy like if the gain is to high. I am thinking that I am not using high enough current for the EVALSTDRIVE101.

How much current did you use to read 0.015 ?

Thanks.

Arnaud