STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1735 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4881 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9578 Views
  • 5 replies
  • 3 kudos

MCSDK 5.Y.4 Download Option Unavailable

This is a website issue, but there was no better category for posting this. The MCSDK download options don't include 5.Y.4. They only include 5.5.x options. This was true in both a Chrome and Edge browsers in Windows 10. https://www.st.com/en/embedde...

WSega.1 by Associate II
  • 2332 Views
  • 2 replies
  • 0 kudos

Hall encoder voltage on STEVAL-SPIN3201

I have an STEVAL-SPIN3201 board and want to connect it to a motor with Hall encoder. According to the user manual, the Hall encoder power supply could be 5V from USB or 3.3V from VDD, setting by JP3 (defaults to USB 5V). In the schematic, Hall signal...

spin3201-sch--3.png