STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to make Websocket Client in STM32CUBEIDE?

I want to make Websocket Client in STM32CUBEIDE and I am using STM32f407 Discovery Board, I have completed the Program with Ethernet(MII, DP83848) with LWP(DHCP enabled) along with FREERTOS. So kindly help me in giving support for the same....

SVerm.3 by Associate III
  • 3149 Views
  • 2 replies
  • 2 kudos

Resolved! X-CUBE-STL difference from ARM's STL

Hi all,I'm doing some research about STLs. What is different between STM's X-CUBE-STL offering and ARM STL Libraries ? Why would you use one over another ?Thank you, best regards

Fnx_QT by Associate III
  • 1541 Views
  • 1 replies
  • 0 kudos

Ethernet Link up, but Ping not working

Using NUCLEO-H723ZG without freeROTS for Ethernet. The link looks working since plugging and unplugging cable indicating "Link Up" and "Link Down". However, the Ping is not working. Not sure any functions need to be called after MX_LWIP_Init()? JYI

JYI by Associate II
  • 2147 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H750 + USB3300 | No signals on ULPI

Hi guys, i am at a complete loss; even with describing the problem.I have a 6-layer board with the USB3300 directly underneath the H750(100Pin LQFP), so traces are short and basically optimal. I use CubeMX to generate an example -> I use MCO2 as 24MH...

Albi G. by Senior
  • 9701 Views
  • 9 replies
  • 1 kudos