I am trying to run STSAFE wrap unwrap example with STM32G484E-EVL but get the following error. I had also included STM32G4 lib files. I am stuck at this point. How should I resolve this error????? Any solution????
Hi Everyone, I had run the example for STSAFE from (STM32CubeExpansion_STSAFE-A_V1.1.1) in that demonstration there are 3 different workspaces I want to ask what is difference between STSAFE_A_using_MbedTLS_CryptoLib & STSAFE_A_using_X_Cube_CryptoLib Which is better in between STSAFE_A_using_MbedTLS_CryptoLib and STSAFE_A_using_X_Cube_CryptoLib
Resolved! Hello everyone I have download the X-CUBE-SAFEA1 Software Package for STSAFE-A software and trying to compile authentication example but get the following error ./Middlewares/ST/STM32_Cryptographic/X509/Inc/x509_crypto.h fatal err #include "crypto.h I don't see any crypto.h file in the entire workspace how will I get this file