STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I'm building a stm32f042 HID device/product, what are my options for updating it 'out in the wild'?

Posted on December 17, 2016 at 20:41The device uses the onboard USB capabilities of the stm32f042 and acts as a HID device.I trying to find the best way to update the device when it is out in the wild, what are my options for doing this?I would want...

USB HS in FS problem with CDC transmission

Posted on December 14, 2016 at 09:59H, I use STM32F439 in HS in FS mode with CDC class. Apparenty even though messages are received by uC  in proper fashion and sent to PC as I coded them,  terminals on PC fail to receive/display them right. If ther...

how to connect usb stick to Nucleo board

Posted on December 16, 2016 at 19:55Hi,I am using NucleoF401re board. I required to connect usb stick to the nucleo. i got following link with guidance. But i don't have LM3526 right now. So, is there any alternative to avoid LM3526 ic.?Or if i conn...

SS.Sagar by Associate III
  • 736 Views
  • 0 replies
  • 0 kudos

STM32 send USB packet bigger than 64B

Posted on December 16, 2016 at 18:16I'm currently developing on a Nucleo-144 (NUCLEO-F446ZE).When i want to send an answer to the pc with a packet bigger than maxpacket (64bytes)the HAL library split it witch is normal but it's not well receive by t...

thom_as by Associate II
  • 725 Views
  • 0 replies
  • 0 kudos

Resolved! STM32F0 timer interrupt frequency speed droping

Posted on December 14, 2016 at 13:59Hello everybody I am using stm32f030F4 in my project and  i need a timer with frequency 200kHzI set timer1 for this frequency and  toggled a pin in timer callback function  and watch with oscilloscope i can see a ...

Flow control with USB CDC or NACKING

Posted on December 14, 2016 at 16:55Hi,I'm trying to figure out a way to emulate UART  RTS / CTS flow control with the USB CDC. My main goal is to be able to tell the host to stop sending data if the �c is busy.After a little googling I come up with...

BDA device with stm32f4

Posted on December 14, 2016 at 09:57hi everyone. im trying to make communication between BDA device(for microsoft) and usb host stm32f4. My device is usb tv. and i wanna take signal from usb port and send this signal to ethernet. Terrestrial ip tv s...