MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Inprove the speed of the ''Mass storage'' as u disk

Posted on March 13, 2012 at 09:30hello everybody,  I was tested using the TF card as a U disk routines.The read speed is 500KB-700KB / s, write speed of 100KB/ s. Too slow, I would like to increase its transmission speed.I will change the way of the...

power3347 by Associate II
  • 5028 Views
  • 15 replies
  • 0 kudos

lsm330dl accelerometer output data problem

Posted on July 03, 2012 at 06:04i'm using the accelerometer in lsm330dl. but when i put the chip statically on the table, the xyz output i got from it is very strange,  for x, it's always between 0.2-0.45  for y, it's always around 1  for z, it's al...

LSM303DLM

Posted on September 08, 2011 at 11:23Hi all, I'm working with LSM303DLM. I have read successfully accelerometer and magnetometer value. Now, i want to use LSM303DLM module as a wakeup device. When my motorbike don't move, the MCU goes to Standby mod...

LIS331HH z-Acc is always zero

Posted on March 19, 2012 at 14:39Hi, i wanna access the acceleration values for the x,y,z axis. So i get a response and values from the registers x (0h28,0h29) and y (0h2A,0h2b), but the register for the z accelerations (0h2C,0h2D) is always zero. A...

iNemo firmware package v2.2.0 hex file

Posted on May 31, 2012 at 18:17Hi, I have been using for some time original iNemo suite application and DFU mode, then I made another program and uploaded it with JTAG programmer.How can I use iNemo suite again?, uploading iNEMOV2_Firmware_PackageV2...

miego by Associate
  • 1293 Views
  • 2 replies
  • 0 kudos

legal rights about SDK code

Posted on May 22, 2012 at 23:54Hi, is it allowed to upload the firmware of my custom inemo application (sportmeter), which based on the SDK of STmicro   to sourceforge ? WR Alex

sam239955 by Associate II
  • 1979 Views
  • 4 replies
  • 0 kudos

L3G4200D angle calculation

Posted on May 24, 2012 at 14:47Hi there,I'm using an L3G4200D sensor for calculating the angle displacementwith the code below. However from the computation I get half of the real rotationthe sensor make, that is, if I rotate it of 90 degree, I meas...

salvatore by Associate II
  • 1231 Views
  • 0 replies
  • 0 kudos

iNEMO 2.x Project in Keil µVision

Posted on April 24, 2012 at 15:38Hi, ist their any iNemo Project already ported in KEIL ? I'm searching for a solution to use the IAR Project in Keil but I always failing when i trying it by my self. with regards Sam

sam239955 by Associate II
  • 1002 Views
  • 1 replies
  • 0 kudos

working with multiple INEMO cards in a MATLAB script

Posted on May 04, 2012 at 14:05hello all! I  am working on my final project in ee studies, and my project requires getting input measurements from 2 INEMO V1 cards at the same script in a MATLAB enviorment. can it be done? and if so, how can I do it...

yakir by Associate
  • 791 Views
  • 0 replies
  • 0 kudos