MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Test

Posted on January 22, 2014 at 17:14Test

fabian by Associate
  • 816 Views
  • 0 replies
  • 0 kudos

LSM303D data synchronization

Posted on January 13, 2014 at 18:35All the example code I've seen reads the acceleration and magnetic field values by polling the appropriate registers.For example:x.l = i2c_read(OUT_X_L_A);x.h = i2c_read(OUT_X_H_A);y.l = i2c_read(OUT_Y_L_A);y.h = i...

trav by Associate
  • 1090 Views
  • 1 replies
  • 0 kudos

Example for LSM303DLHC Accelerometer

Posted on November 27, 2013 at 15:26Hi,I need to read the accelerometer data from LSM303DLHC. I use the STM32F401 Discovery board and the ''stm32f401_discovery_lsm303dlhc.c'' library.I read carefully the datasheet, especially the section 7.1 in page...

anthony2 by Associate II
  • 3206 Views
  • 6 replies
  • 0 kudos

L3GD20 gyroscope sensitivity

Posted on January 14, 2014 at 11:04Hi,I would like to know : how did you calculate the L3GD20 sensitivity (LSB/dps) in the example?#define L3G_Sensitivity_250dps    (float)114.285f        /*!< gyroscope sensitivity with 250 dps full scale [LSB/dps] ...

romain by Associate
  • 918 Views
  • 0 replies
  • 0 kudos

INemo Engine Lite

Posted on January 13, 2014 at 10:10Hello, In the iNemo Engine Lite Version 1.2.0 (FW V.2.3.0) when analizing the EKF Prediction state I came to the conclusion that the quaternion update is not using the same mathematical function defined by the pMa...

stst9193 by Associate II
  • 714 Views
  • 0 replies
  • 0 kudos

CS43L22 and LSM303DLHC

Posted on December 23, 2013 at 15:01I would like to configure both the CS43L22 Audio DAC and the LSM303DLHC MEMS accelerometer to be used simultaneously. From what I have seen on the documentation, it seems that both of these devices are connected t...

Behavior of LIS3DH past range limits

Posted on December 13, 2013 at 19:45If the LIS3DH range is set to +/- 2g, how does the chip behave if acceleration exceeds 2g's? Do the axis outputs limit, wrap around, go to some fixed value, etc?

cbrower by Associate
  • 698 Views
  • 1 replies
  • 0 kudos