cancel
Showing results for 
Search instead for 
Did you mean: 

Behavior of LIS3DH past range limits

cbrower
Associate
Posted on December 13, 2013 at 19:45

If the LIS3DH range is set to +/- 2g, how does the chip behave if acceleration exceeds 2g's? Do the axis outputs limit, wrap around, go to some fixed value, etc?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Thiago REIS
Associate II
Posted on January 10, 2014 at 14:21

Hello Charles,

the output value will show the maximum value allowed by that full scale.

In this case, for 2g, if you apply a 4g acceleration, the output will show the maximum of 2g.

Thank you,

Thiago Reis