MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

installing the iNemo2 firmware

Posted on February 26, 2011 at 04:53 Hi Folks, I bought the iNEMO V2 evaluation board. It has the demostration firmware on it. I would like to use this board as a complete system since it has all the sensors on it. So, will I be able to inst...

kirank by Associate II
  • 1599 Views
  • 8 replies
  • 0 kudos

firmware

Posted on July 14, 2011 at 07:08doas anyoane know, if the new ''iNemo-Engine'' is already available ? And if, where is it available?  Or when is it ? Which is the chip-configuration for this engine? LSM303DLM + L3G4200G ? #inemo-engine

Development tool

Posted on May 26, 2011 at 12:21Hello, I'm trying to open iNEMO v2 firmware with IAR Embedded Workbench for ARM 6.20, but during building a houndreads of errors appears. Now I'm wondering if I use the proper tool for development of firmware. If anyon...

eleandir by Associate
  • 1043 Views
  • 1 replies
  • 0 kudos

Question regarding iNEMO output modes

Posted on May 27, 2011 at 19:54I have questions regarding the configuration output data for the iNEMO board v2. Based on the iNEMO2_SDK.h header file, I know that the following output modes can be defined: - Default output mode - Raw output mode - A...

dgh by Associate
  • 877 Views
  • 3 replies
  • 0 kudos

STM32W

Posted on July 13, 2011 at 11:16Can somebody tell me, what prebuild firmware is loaded in the two kit-parts in this specific demo? http://www.youtube.com/watch?v%3Dz3f4n9s3Kug The GUI seems to be EK302DL Thank's

Components of iNEMO v2

Posted on July 06, 2011 at 16:33First I say Hello to all! Sorry for my english, it's not my native language. I wonder why iNEMO v2 uses two of ANALOG gyro if STm now has complete 3-axis digital solution (L3G4200D)? why its not used, what advantages ...

MKI062V1 FW version & BufferUsage function

Posted on May 18, 2011 at 07:48I'm trying to acces the FW Version & BufferUsage information of iNEMO .Please have a look at attached .cpp file (works for streaming data from iNEMO) .The BufferUsage function is very important for me since, I'm going ...

harinath by Associate III
  • 828 Views
  • 3 replies
  • 0 kudos

MKI062V1 MATLAB wrapper( unloadlibrary problem)

Posted on May 25, 2011 at 03:45Hi friends,With deep interest and many trials, I could be able to connect iNEMO V1 to MATLAB. Your can see the attached INEMO_ConnectionV1.m working code. I commentedunloadlibrary('iNEMO_SDK')  which is making MATLAB u...

harinath by Associate III
  • 796 Views
  • 0 replies
  • 0 kudos

Problem with DFU mode.

Posted on May 20, 2011 at 10:28Hello,I have problem with updating firmware in STEVAL-MKI062V2. According to manual to update it I have to switch board into DFU mode, but system doesn't see the device in this mode. Below I wrote out in few steps what...

eleandir by Associate
  • 960 Views
  • 1 replies
  • 0 kudos