MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How are people compiling iNemo code???

Posted on January 27, 2012 at 00:59Has anyone successfully compiled any of the iNemo/DFU code?  If so, how did you do it?I've tried Atollic/eclipse, which wouldn't work because there's no project file and I couldn't seem to resolve the dependencies ...

jake by Associate II
  • 638 Views
  • 1 replies
  • 0 kudos

Compiling on Atollic, or anything other than IAR ?!?

Posted on January 26, 2012 at 23:23I can't get DFU or iNemo firmware code to compile with Atollic.The code seems to be a mess with changes to the standard libraries, etc..  Please create a project file for Atollic, or tune up the code so it will com...

jake by Associate II
  • 947 Views
  • 1 replies
  • 0 kudos

L3G4200D Teperature Data

Posted on December 01, 2011 at 19:46How I can interpret the temperature data from the Gyroscope L3G4200D? I can't find anything about the OUT_TEMP Data reference �C. I know, the range is -40 to 85�C. #l3g4200d #mems #l3g4200d #support

FIFO timing Error

Posted on December 20, 2011 at 20:27I am facing timing issue with lis3dh accelerometer in FIFO mode.Currently my ODR=25 Hz and I am reading FIFO on watermark threshold=30.As soon as I get watermark interrupt I read 196 (32*3*2)samples at 5 Mhz.Hence...

software problem iNEMOEngine LI3

Posted on January 17, 2012 at 08:02Hi ST-team,i have downloaded the iNEMOEngine LI3 software. After the registration I get the link to download the file with the name: ''iNEMO_Suite_2.3.0_110913.zip''. When I try to open it I get an error message th...

nikolaj by Associate
  • 507 Views
  • 1 replies
  • 0 kudos

STeval-MKI 109V1, also V2

Posted on December 29, 2011 at 11:04Hi,I intend to use several STeval-MKI109Vx structures, up to ten systems, simultaneously, andall of them ''wireless''. STM offers a wireless Bluetooth kit for connecting to STeval-MKI109V1.Is it possible to use up...

Ploblem with JLINK and iNemo broad

Posted on December 06, 2011 at 11:42Hi,I met this problem, iNemoand computerconnectionssuggested that ''could notdistinguish between USBdevices, '' First of all, I wanted to step through the code line by line with JLINK, under the RDI mode, But aft...

dxpfigo by Associate
  • 518 Views
  • 0 replies
  • 0 kudos

Problem with SD card interface on Inemo

Posted on August 16, 2011 at 14:32Hello,         Im facing a problem with the Inemo SDcard api. Iam able to read and write multiple blocks and single blocks but Im not able to erase the card. When I issue a command for erase and then read the block ...

Spruce -SolidDigi STM32 Arduino Compatible Board With LCD

Posted on November 02, 2011 at 10:25Spruce -SolidDigi STM32 Arduino Compatible Board With LCDSpruce -SolidDigi STM32 ARM cortex board can be used with http://www.cutedigi.com/product_info.php?products_id=4408 and is compatible with http://www.cutedi...