MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Question about LIS3DH acceleration data

Posted on January 27, 2015 at 06:47 1) Question1 I am reading the the data sheet of LIS3DH AN3308.  I doubt about the description of 3.2.3(Example of accleration data).350(0x15E)mg register data is Val_0x29 = 0x15, Val_0x28 = E0 (left-justified)It i...

xia by Associate
  • 1068 Views
  • 1 replies
  • 0 kudos

LPS331AP reference software

Posted on November 06, 2014 at 05:43I have been having some trouble getting up and running with the LPS331AP. Using a logic analyzer, I've verified that the sequence of commands given in AN4159 section 5.1.1 (one shot mode measurement sequence) is b...

crwper by Senior
  • 886 Views
  • 1 replies
  • 0 kudos

LSM9DS0 gyro accuracy

Posted on January 27, 2015 at 09:55What is LSM9DS0  gyro accuracy? (bias instability, Allan variance, etc..) In this forum http://forum.taulabs.org/viewtopic.php?f=22&t=200 the user http://forum.taulabs.org/memberlist.php?mode=viewprofile&u=108 sai...

LIS3DSH - Sampling Synchronization

Posted on January 22, 2015 at 14:55Hi all, I'm currently evaluating the LIS3DSH for an integration in a multi-sensor monitoring system. I need to enforce synchronization of sampling between all the digitals sensors of the system but I didn't found ...

timothe by Associate
  • 839 Views
  • 0 replies
  • 0 kudos

LIS3DSH DATA FORMAT

Posted on November 17, 2014 at 11:45I get wrong accelerometer's values. I have concatenated xMSB+xLSB, yMSB+yLSB and zMSB+zLSB. Then I verify if the resulting valor is negative, in such case I substract 2^16 to convert from 2's complement number to ...

jbeltran by Associate II
  • 2368 Views
  • 6 replies
  • 0 kudos

LSM303DLHC accelerometer - is data register left justified?

Posted on November 26, 2014 at 06:40Hi I configured the LSM303DLHC accelerometer as follows. CTRL_REG1_A with 0x77  //400hz data CTRL_REG4_A with 0x00 //Little endian And started reading the data from the OUT_X / Y/ Z_L / H_A registers. But I could ...

LSM9DS0 SPI trouble STM32F405

Posted on November 07, 2014 at 08:45Hi everyone,this is my SPI configuration used for interfacing with the LSM9DS0 in 4 wire RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI2 , ENABLE);    SPI_InitStruct.SPI_Direction = SPI_Direction_2Lines_FullDuplex;    ...

tylere by Associate II
  • 1195 Views
  • 1 replies
  • 0 kudos

How to get the STEVAL-MKI121V1 board to work under Linux?

Posted on January 19, 2015 at 16:24I can get the STEVAL-MKI121V1 to work under Windows via the Inemo SDK. I would like to have a similar setup under linux. Is there a driver (module) and SDK available to do the same?What would be the fastest and eas...

amanders by Associate
  • 910 Views
  • 0 replies
  • 0 kudos

l3gd20, FIFO level

Posted on January 16, 2015 at 13:28Hello.What i am trying to do - is to synchronize all inertial sensors (accel, gyro, mag). Each of these sensors has its own FIFO buffer.I did not encounter any problems with magnetometer and accelerometer, in contr...

sir by Associate
  • 768 Views
  • 0 replies
  • 0 kudos

STEVAL-MKI117V1 audio output

Posted on January 12, 2015 at 16:48Hi, I'm runnig a small research project with the STEVAL-MKI117V1 evaluation board. At the moment I'm facing some problems with accessing the audio data stream. Hopefully someone can answer my questions: 1. Is it p...