MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LPS25H power consumption

Posted on June 16, 2015 at 08:38Hi, I use LPS25H in my project. Based on the application note AN4450 page 13,(example 1) when I configure the LPS25H to the mode that ODR is 25 Hz,  pressure average 512, temperature average 64 (register 0x20 is 0xC0,...

hitwch by Associate II
  • 1144 Views
  • 1 replies
  • 0 kudos

LIS3MDL axis swap and inversion

Posted on July 23, 2015 at 11:57Hi,I'm using LIS3MDL for a while now and I recently encountered a problem on the sensors detected via the self test option.Some of the sensors I'm using began to give me some strange data. As far as I understand the p...

guilhem by Associate
  • 680 Views
  • 0 replies
  • 0 kudos

MEMS LPS25H read always 0x1E

Posted on June 13, 2014 at 04:14use MCU SPI MODEL , I have used oscillometer test.write @0x20=0x00read  @0x20=0x1ewrite @0x20=0x84read  @0x20=0x1eerror... 

0690X00000603DWQAY.jpg
plls2011 by Associate
  • 1461 Views
  • 4 replies
  • 0 kudos

Symbol & Footprint

Posted on July 20, 2015 at 18:26Although this is an old post, thought I'd chime in here in case it's useful for anyone else going forward. The LSM330D accelerometer symbol/footprint is available for download here -- just select Altium as the downloa...

natasha by Associate
  • 847 Views
  • 0 replies
  • 0 kudos

sometimes Laser switch off

Posted on July 20, 2015 at 17:40Hello, the VL6180X Sensor is in continuous mode, I am polling Interrupt_status_gpio. Sometimes the Laser switch off and the Interrupt_status_gpio is always 0x00. Vcc is 2,8V. Whats the problem?

guenter by Associate
  • 684 Views
  • 0 replies
  • 0 kudos

H3LIS331DL interrupt duration

Posted on July 13, 2015 at 19:57Hello, I am working with the STEVAL-MKI153V1  eval board and have configured interrupt 1 to be the ''data ready'' interrupt. My question is how do I calculate the interrupt duration? All the data sheet says is it is c...

ressen01 by Associate
  • 700 Views
  • 0 replies
  • 0 kudos

LSM303DLHC DRDY signal

Posted on July 10, 2015 at 17:34 LSM303DLHC Data Sheet says The LSM303DLHC features two data-ready signals (RDY) which indicate when a new set of measured acceleration data and magnetic data are available but Figure 4 only shows...

LIS2DH decoupling Capacitors

Posted on July 08, 2015 at 21:37On the data sheet it is recommended to add 3 capacitors to the system. '' The device core is supplied through the Vdd line while the I/O pads are supplied through the Vdd_IO line. Power supply decoupling capacitors (1...

nir23 by Associate
  • 990 Views
  • 0 replies
  • 0 kudos

LIS331HH data rate

Posted on July 08, 2015 at 14:00Hello, does anybody know how accurate the data rate of the LIS331HH sensors should be? I use two with a data rate of 1000Hz of them and want to synchronize the measurment results. For this reason i measured the Interr...

bognermn by Associate
  • 656 Views
  • 0 replies
  • 0 kudos

Lsm9ds0 interrupt delay issue

Posted on July 06, 2015 at 14:49I am using Lsm9ds0 device connected to imx6 processor via i2c with following configuration. Set Gyro ORD to 95hz. Set Watermark level to 30 Set to Stream mode register configuration {CTRL_REG3_G, 0x04},     {CTRL_REG4...

sijilcv by Associate
  • 708 Views
  • 0 replies
  • 0 kudos