MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM303DLHC Soft Iron and Hard Iron Caliberation

Posted on November 28, 2014 at 06:41Hi,I am using LSM303DLHC device to make a tilt compensated magnetic compass. In my PCB there is some disturbance due to the presence of other components. I saw in an application note (AN3192) we can apply soft iro...

shiju by Associate
  • 627 Views
  • 0 replies
  • 0 kudos

Finger Prints detection

Posted on November 27, 2014 at 08:34Hello, Is there any ST product available for Human Finger Prints detection ? Thanks, Vani

LIS3DSH

Posted on November 26, 2014 at 23:14I am trying to implement a state machine that looks for a peak above a threshold.I got the threshold part working, but can't seem to get anything on the Peak detection register. Does anyone have a set up that work...

jin1 by Associate
  • 433 Views
  • 0 replies
  • 0 kudos

LSM303D Problem

Posted on November 23, 2014 at 12:24Hi,We are working on a temperature logger application, We are using LSM303D as accelerometer in our application to wake up system on movement. We have interfaced it over I2C lines, there are few other sensors on I...

pratik2 by Associate
  • 648 Views
  • 1 replies
  • 0 kudos

LIS3DH not outputting any X data

Posted on November 21, 2014 at 07:34Hi,For some reason, the X channel is not working.Here are my configurations for each config register: send[0] = 0b01100000;//start config send[1] = 0x57;//reg 1 send[2] = 0x00;//reg 2 send[3] = 0x00;//reg 3 send[4...

ethan by Associate
  • 611 Views
  • 1 replies
  • 0 kudos

303C

Posted on November 21, 2014 at 06:02Is there a users guide or something more than the thin data sheet?I need some basic set up examples, andneed to know how to calibrate for hard iron! #303-c-calibrate

tim23 by Associate
  • 491 Views
  • 0 replies
  • 0 kudos

.

Posted on November 19, 2014 at 13:11

rnd23 by Associate
  • 621 Views
  • 1 replies
  • 0 kudos

LIS3DH wrong behavior after writing to CTRLREG6

Posted on November 18, 2014 at 19:53Hello,Some day ago I've started work with LIS3DH accelerometer. Everything works fine -Reading accelerations, highpass filter, low power mode and INT1 interrupt line.At start INT1 was configured as high when activ...

radoslaw by Associate
  • 528 Views
  • 0 replies
  • 0 kudos

impat detection using lis3dsh sensor.

Posted on November 15, 2014 at 08:55hi i m using lis3dsh sensor to detect the accidents. for this i need to detect the impact using the variation of the G value.. from sudden shift of 2g to around 16 g and also fall detection .. so far i am getting ...

n.serina by Associate III
  • 519 Views
  • 0 replies
  • 0 kudos

Data ready interrupt on lsm303d

Posted on November 14, 2014 at 20:55Hi i was trying to enable the data ready on accelerometer .however i'm not sure how to check whether it's enabled or not .i mean whenever i read the value in IG_SRC2 it shows that 0x00 also i have not enabled the ...