MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Could not achive 3200Hz data rates for ADXL345 with Nucleo-L053R8

Posted on November 03, 2015 at 10:27Hi,I'm planning to get 3200Hz data rates for ADXL345 sensor with Nucleo board. The SPI speed is 5MHz. And i initialized exactly as per the data sheet.the initialization process is as below:accelerometer.setPowerCo...

gandhi by Associate II
  • 859 Views
  • 0 replies
  • 0 kudos

HAL drivers for lsm6ds3 with STM32F1 series?

Posted on November 02, 2015 at 22:59Hello, We couldn't find any firmware source code example for STM32F1 series support with in STM32CubeExpansion_MEMS1_V1.4.0 .Is there such HAL drivers for lsm6ds3 with STM32F1 series 32 bot controllers?Thanks, ...

suresh by Associate II
  • 817 Views
  • 0 replies
  • 0 kudos

LPS331AP - SPI mode - Multiple slaves sharing common SPI bus

Posted on October 07, 2014 at 19:06We are planning to use LPS331AP in one of our design. LPS331AP will be interface to MCU using 4-wire interface. I could not find conclusive information on whether Data out (pin 7) is tri-stated/high impedance when ...

sumeet by Associate
  • 1385 Views
  • 2 replies
  • 0 kudos

Wrong output 0 0 0 or -1 -1 -1 for ADXL345 accelerometer in SPI

Posted on October 27, 2015 at 12:42Hi,I'm programming the ADXL345 3-axis sensor for my thesis project. Initially i made the program in I2C and its working fine. Later on i switched to SPI mode for better speeds. Unfortunately the device is not worki...

gandhi by Associate II
  • 736 Views
  • 0 replies
  • 0 kudos

LIS3MDL high nonlinearity for negative magnetic fields

Posted on September 16, 2015 at 11:35Hi all, I am testing a board that uses a LIS3MDL as a magnetic reference sensor communicating with a 3-wire SPI. I am testing the sensor using a Helmholtz coil that I built (that, by the way, has been tested and ...

jose2399 by Associate
  • 872 Views
  • 1 replies
  • 0 kudos

LIS3DH chip marking

Posted on October 21, 2015 at 04:18HiDoes anyone know what the correct chip marking for the LIS3DH(TR) should be? I've seen many different markings, incl. 2220 C3H 8F2CB. However, mine has this marking http://i.imgur.com/1OyaTUe.pngSo is there a cor...

munddr by Associate
  • 1257 Views
  • 0 replies
  • 1 kudos

Where can I find AIS326DQ failure modes/rates?

Posted on October 16, 2015 at 15:10Hello everyone.Does anybody know where can I find AIS326DQ failure modes/rates?Datasheet does not help much.And, may be the arrangement of the physical sensors (i.e., whether it is a combination of three independen...

LIS3DSH w/ STMF4 Discovery Board

Posted on October 08, 2015 at 15:52I've recently purchased the STMF4 Discovery Board and am looking to write an application making use of the on board LIS3DSH accelerometer. However, the examples provided (and pointed to by the documentation) all ma...

iNEMO boards not detected by PC(win-7 64 bit)

Posted on October 06, 2015 at 14:20Hi ,We have bought inemo sensors and made connection as per the datasheet. We made usb connection(without ESD protection) and provided jumper for boot mode.I have installed inemo-suite which does driver installatio...

nishal by Associate
  • 729 Views
  • 0 replies
  • 0 kudos

MEMS mics into the musical instruments pickup systems

Posted on October 05, 2015 at 20:55My name is Mikheil Tsitsishvili, I am acoustic guitar and ukulele performer living in the Republic of Georgia (East. Europe). I am very much interested in the amplification of acoustic instruments; all my instrumen...