MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM6DS3 gyro data is off by about 15% of what I expect

Posted on February 25, 2016 at 19:26Greetings.I am trying to get accurate gyro data out of the LSM6DS3, but my results are about 15% off of what I expect.  My test setup is a PASCO scientific Rotary Motion Sensor (RMS) with a LSM6DS3 mounted on top ...

wild by Associate II
  • 1120 Views
  • 1 replies
  • 0 kudos

LIS3DH Power Consuption

Posted on March 17, 2016 at 07:15Hi! I am not getting anywhere near the Power Consuption specifications. I see a minimum power off 100uA, and no way to cut it down. According to documentation this device start in Power Down until any register is man...

rvalle by Associate
  • 699 Views
  • 0 replies
  • 0 kudos

Getting the timestamp of the Sensor Data Sample Precisely

Posted on March 16, 2016 at 19:01LSM6DS3 has a dedicated register for the timestamp like -> TIMESTAMP1_REG (41h)/TIMESTAMP2_REG (42h) .But apart from this sensor how can the time stamp of a every data sample be captured of any sensor.By reading the ...

darla14 by Senior
  • 865 Views
  • 0 replies
  • 0 kudos

Any issues using LIS3DH direct from coin cell unregulated power?

Posted on March 16, 2016 at 17:15The LIS3DH works from 1.8V to 3.6V.If I use it direct from a CR2032 coin cell w/o regulator, will there be any side effects as the voltage drops from 3.3V to ~2.2V?For example, will the calibration drift substantiall...

duppy by Associate
  • 823 Views
  • 0 replies
  • 0 kudos

STM32F4 Discovery to LPS25H Example Code

Posted on July 22, 2015 at 14:08All:Is there I2C example code that can be used with the STM32F4 Discovery Board to connect to the LPS25H module? I am running the processor at the full 168 MHz, and as far as I know, I have initialized the I2C1 port c...

tba10596 by Associate II
  • 2481 Views
  • 5 replies
  • 0 kudos

Using LIS3DH direct from coin cell unregulated power

Posted on March 15, 2016 at 17:48The LIS3DH works from 1.8V to 3.6V.If I use it direct from a CR2032 coin cell w/o regulator, will there be any side effects as the voltage drops from 3.3V to ~2.2V?For example, will the calibration drift substantiall...

duppy by Associate
  • 775 Views
  • 0 replies
  • 0 kudos

LIS2DH12 INT1 configuration & calculate decimal value of xyz axis

Posted on March 15, 2016 at 10:29Hi Guys,I need to print XYZ axis data whenever their is raise in INT1 with FIFO buffer. And one more thing i'm getting temperature and XYZ data without INT1 but those value are in hexadecimal how can i get in normal ...

ganesh by Associate
  • 932 Views
  • 0 replies
  • 0 kudos

LIS3DSH scale offset

Posted on March 11, 2016 at 07:21There is a problem with LIS3DSH scale offset. We calibrate our devices for 1000 mG and -1000 mG, using raw data from accelerometer. After 1 month warehouse storage at room temperature, difference between values is st...

mila by Associate
  • 828 Views
  • 0 replies
  • 0 kudos

STEVAL-IME002V1 problems

Posted on September 17, 2015 at 15:47Hope that this is the correct forum section for my question. I have some strange problems with my IME002V1 evaluation kit. When I change some register settings in the Eden application and press write all register...