MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to download iNEMOEng_M1LI3 source code ?

Posted on April 01, 2016 at 15:09Either from http://www.st.com/web/en/catalog/tools/FM147/CL1818/SC1528 or http://www.st.com/web/catalog/tools/FM147/CL1818/SC1528/PF260129♯ it is impossible to download the source code to port on STM32L4 and support...

Noyb by Associate II
  • 821 Views
  • 0 replies
  • 0 kudos

LSM6DS0 interrupt configuration issues

Posted on March 31, 2016 at 08:19I need help to configure the interrupt, specifically for a 6d orientation interrupt. I have working as needed a light touch interrupt on any axis, but I also need sometimes to configure to interrupt only on a transit...

LIS3DH and fall detection

Posted on November 12, 2013 at 04:12I have used the LIS3DH for movement and angle detection for about 18 months. I now wish to use it for fall detection. Previously I ued another brand where you setup a register and get an interrupt when a zero G oc...

martech by Associate II
  • 2330 Views
  • 4 replies
  • 0 kudos

LIS3DH INT2 Configuration

Posted on June 07, 2015 at 19:15Hi,For LIS3DH, the datasheet mentions two user programmable interrupts INT1 and INT2. Though config, threshold, duration etc. (INT1_CFG, INT1_SRC, INT1_THS, INT1_DURATION) registers are listed for INT1, no such regist...

rihana by Associate
  • 2065 Views
  • 3 replies
  • 0 kudos

Incorrect FIFO alignment

Posted on March 27, 2016 at 01:02I am running the LSM6DS3 in continuous FIFO mode capturing gyro and acc data. While collecting data I periodically pole to see if the water mark is met (96 words), and if so read out half of them (leaving some in the...

mikem by Associate
  • 807 Views
  • 0 replies
  • 0 kudos

STM32F429 Audio USB with CubeMX

Posted on May 06, 2015 at 13:02Hello, I have a quick question, and I cannot find answer anywhere on the web (including Reference Manual for MCU). I'm preparing for a new project, picking master unit, where one of most important feature is USB audio ...

axel2 by Associate II
  • 3325 Views
  • 4 replies
  • 0 kudos

VL53L0 - How it works

Posted on March 08, 2016 at 15:40Do you have any plans to release a version of this sensor with a smaller FieldOfView?As your presentation note you use a kind of diode matrix as photon input, do you plan to output the data of each diode to identify ...

ee06091 by Associate III
  • 1083 Views
  • 1 replies
  • 0 kudos

LSM6DS3 gyro data is off by about 15% of what I expect

Posted on February 25, 2016 at 19:26Greetings.I am trying to get accurate gyro data out of the LSM6DS3, but my results are about 15% off of what I expect.  My test setup is a PASCO scientific Rotary Motion Sensor (RMS) with a LSM6DS3 mounted on top ...

wild by Associate II
  • 1078 Views
  • 1 replies
  • 0 kudos