how to tell if the LSM330 chip is dead
Posted on June 08, 2013 at 00:27My LSM330 chip is not responding to SPI communication. Is there a way to electrically tell if the chip is dead? Thanks.
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Posted on June 08, 2013 at 00:27My LSM330 chip is not responding to SPI communication. Is there a way to electrically tell if the chip is dead? Thanks.
Posted on January 10, 2014 at 07:53I am sorry that I post a question about pressure sensor at accelerometer forum, but I can't find a forum about barometric pressure sensor. I hope to know the wake up time of the chip from the power down to ready st...
Posted on July 23, 2014 at 16:56I am looking for the best option versus this ADI part. Key requirements are - powered by 3.6V DC.- zero g temperature stability of 0.1 mg/C or better.- resolve angles down to 0.5 degrees at least, 0.1 degrees preferre...
Posted on July 21, 2014 at 18:30I wanted too know if it is possible to use the pro version of the engine on the M1 module, is the hw compatible?Thanks for the help
Posted on July 20, 2014 at 11:01H3LIS331DL accelerometer has 3-wire SPI mode. What i will get in this (3-wire) mode at pin number 7 (SDO in 4-wire mode). Is it pull down, pull up or open drain ?
Posted on July 19, 2014 at 15:18Transferring my life to a new machine and can't find the mini-CD that came with this eval kit.Does anyone know if it's available online and where?Thanks,Geoff #accelerometer
Posted on June 29, 2014 at 17:20Morning, everyone,I used a demonstration board STEVAL-MKI062V2. I wrote a small C++ program and want to get data from the sensor. It looks like, that some functions are not in the dll file (''iNEMO2_SDK.dll'') .The co...
Posted on July 16, 2014 at 11:59Dear all,I'd like to configure the LIS3DH in order to enter my uc in sleep mode in a certain position P0 and then be awaken when the position move from P0 +/- threshold.I dont want to detect a movement but a position ...
Posted on March 25, 2014 at 22:50The data sheet makes no explicit mention of a way to force this interrupt to latch and clear when the CLICK_SRC register is read (like the INT1_CFG registers can).App note AN3308 states that this behavior can be achi...
Posted on June 18, 2014 at 11:54Hi guys,I have jsut started using the Inemo_m1 discovery board.After Installing the software and doing some hello world projects (using KEIL IDE;debugged via ST-Link debugger), I decided to setup communication with th...