MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

IIS2DH data convert data to g

Posted on June 06, 2016 at 03:14I'm using IIS2DH, I config it to normal mode, so It's 10bit resolution, and I got 16bit data for each axis, now I right shift the 16bit data to get a 10bit data, and the range is 0-1023, is that right? but And if I k...

LIS3DHTR interrupt pins

Posted on May 25, 2016 at 14:09Hello guys, I'm planing to use LIS3DHTR accelerometer in my next project. There is one thing (for the moment :-)) that is bothering me: The default state of the INT1 and INT2 pins is not explicitly indicated within a d...

bojan by Associate II
  • 708 Views
  • 1 replies
  • 0 kudos

STEVAL-MKI159V1 connection to Raspberry PI 3

Posted on May 25, 2016 at 18:57Hello everyone. This is my first posting on this forum. I am an electrical engineering major completing a senior design project. I am designing a smartwatch and I purchased the STEVAL MKI159V1 motion sensor and this wi...

jigle004 by Associate
  • 725 Views
  • 1 replies
  • 0 kudos

Sensor Controller Studio with LPS22HB

Posted on June 27, 2016 at 15:50Hi everyone,I'm working on LPS22HB and I use Sensor Controller Studio (a TI's tool).Do anyone in this forum used this Studio? We can exchange knowledge and experience. Best,Dung. #lps22hb #ccs #scs

le by Associate II
  • 474 Views
  • 0 replies
  • 0 kudos

Downscale range

Posted on June 23, 2016 at 05:04Is it possible to down scale the range by 2 to 50mm and output in 0.5mm increments represented as integers in a similar way upscaling works?

USB AUDIO DRIVER QUESTION

Posted on June 22, 2016 at 16:17 Hi guys, Sorry that I have a dumb question I am new to STM32's board, and we are currently using  F446 with MEMS microphone module. We want it act as a USB microphone like what it said.   http://www.st.com/content...

cks7788 by Associate II
  • 464 Views
  • 0 replies
  • 0 kudos

Mems microphones frequency response

Posted on September 28, 2015 at 16:38Hello,I�m using an stm32f4-discovery board and I�m trying to sample the on board mems microphone at 48 kHz. I record a large number of samples and send them to the computer via USB (if someone knows a better way ...

rjrg1989 by Associate
  • 1061 Views
  • 2 replies
  • 0 kudos

LPS25HB Temperature Compensation Behavior

Posted on May 09, 2016 at 19:52My colleagues and I are evaluating the LPS25HB and came across some behavior we don't understand. There are two issues we are trying to resolve right now: Embedded temperature compensation behavior is confusing.Accur...

kris2 by Associate
  • 1807 Views
  • 4 replies
  • 0 kudos