MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

lps22hb no pressure and temperature response

Posted on December 11, 2016 at 07:25I have connected LPS22HB development kit (STEVAL-MET001V1) and Raspberry Pi 3 with I2C interface and tried to read pressure and temperature data but whatever setting I tried, pressure (0x28, 0x29, 0x2A) and temper...

Free-fall and motion detection simultaneously on LIS3DH

Posted on November 29, 2016 at 23:46Hi support,We wonder if there is any register configuration that allow us to route the motion detection to the INT1 pin and the free-fall detection to the INT2 pin and both working at the same time? Both pins are ...

jgaldana by Associate II
  • 990 Views
  • 1 replies
  • 0 kudos

LIS3DHTR data length

Posted on November 02, 2016 at 07:41What is the actual data (x,y,z) length. When I'm reading the acceleration data , the lowest 4 bitsare 0. This would indicate the data is actually 12bit , left justified. The datasheet however say's the FIFO is 10b...

Rob1 by Associate II
  • 1406 Views
  • 2 replies
  • 0 kudos

X-CUBE-MEMSMIC : Extension to 6 microphones

Posted on January 12, 2016 at 15:18Hello, I need help with regard to extending the 4 microphone architecture of X-CUBE-MEMSMIC to 6 microphones using X-NUCLEO-CCA02M1 and STEVAL-MKI155V3. I have attached the modified BSP driver .c and .h files. Also...

MP23DB01MM datasheet

Posted on September 07, 2016 at 10:40Hello,I saw that MP23DB01MM is used in BlueCoin  device. I would like to investigate this microphones characteristics but  could not find a data sheet. Please could you redirect me to data sheet web page ?Thanks ...

LIS2DH12 Movement Interrupt configuration

Posted on October 03, 2016 at 18:31Good morning, I'm having a heck of a time trying to get my configuration settings correct on my LIS2DH12 Accelerometer.I would like it to fire the interrupt when an abrupt movement occurs on any or all axes.I have ...

LSM6DS33 supply voltage

Posted on November 23, 2016 at 11:58Hi,The typical supply voltage for the LSM6DS33 is 1.8V and the maximum limit is 3.6V. Is it fine if a supply voltage of 3.3V is continously provided to the device?Regards,Prachi  #lsm6ds33

prachi by Associate
  • 938 Views
  • 1 replies
  • 0 kudos

LSM6DS33 SPI pin functions

Posted on November 25, 2016 at 04:59Hi,As per the datasheet, the pin &sharp3 of the LSM6DS33 device is used as 1. I2C serial data (SDA)2. SPI serial data input (SDI)3. 3-wire interface serial data output (SDO)In what SPI mode is it used as an input ...

prachi by Associate
  • 1134 Views
  • 1 replies
  • 0 kudos