MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Downscale range

Posted on June 23, 2016 at 05:04Is it possible to down scale the range by 2 to 50mm and output in 0.5mm increments represented as integers in a similar way upscaling works?

USB AUDIO DRIVER QUESTION

Posted on June 22, 2016 at 16:17 Hi guys, Sorry that I have a dumb question I am new to STM32's board, and we are currently using  F446 with MEMS microphone module. We want it act as a USB microphone like what it said.   http://www.st.com/content...

cks7788 by Associate II
  • 439 Views
  • 0 replies
  • 0 kudos

Mems microphones frequency response

Posted on September 28, 2015 at 16:38Hello,I�m using an stm32f4-discovery board and I�m trying to sample the on board mems microphone at 48 kHz. I record a large number of samples and send them to the computer via USB (if someone knows a better way ...

rjrg1989 by Associate
  • 1002 Views
  • 2 replies
  • 0 kudos

LPS25HB Temperature Compensation Behavior

Posted on May 09, 2016 at 19:52My colleagues and I are evaluating the LPS25HB and came across some behavior we don't understand. There are two issues we are trying to resolve right now: Embedded temperature compensation behavior is confusing.Accur...

kris2 by Associate
  • 1698 Views
  • 4 replies
  • 0 kudos

Datalogger Application for Non Motion Sensors

Posted on June 15, 2016 at 12:24There is a utility for MEMS data logging in the Nucleo Packages but is there any Utility for datalogging Other sensors like UV Sensors and Mems MicroPhone Sensors?Eagerly waiting to know on this? #mems-microphone-a...

darla14 by Senior
  • 496 Views
  • 1 replies
  • 0 kudos

hts221 SPI driver

Posted on June 05, 2016 at 03:20hi, I'm using the HTS221 humidity and temperature sensor along with the STM32F205. They are connected over the SPI bus but I am unable to get the STM32F205's SPI communications working correctly. Can anyone recommend ...

doug2399 by Associate
  • 641 Views
  • 1 replies
  • 0 kudos

ST Motion Sensor

Posted on June 14, 2016 at 20:48Hello. I am designing a smartwatch prototype and recently purchased the MKI159V1 which has the LSM9DS1. My company is still under construction. I noticed I am having a little trouble finding the link for the software ...

jigle004 by Associate
  • 482 Views
  • 0 replies
  • 0 kudos

VL6180x working environments

Posted on June 13, 2016 at 17:33Can the VL6180x sensor work perfectly fine in both indoor and outdoor environments? Does the amount of light present in the environment affect the operation of the time of flight sensor?