MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LPS25HB data reading 6.4mBar Offset Error

Posted on August 25, 2015 at 13:12​Hi,I working with Barometric Pressure sensor LPS331AP.Its working good. but as this chip absoluted,then we changed design to LPS25HB.But this chip is reading 6.4mBar error apart from the actual measured value .We a...

satyag by Associate II
  • 1875 Views
  • 3 replies
  • 0 kudos

lsm6ds3 Accelerometer theoretical accuracy

Posted on February 08, 2017 at 21:16Good afternoon,I am trying to determine the theoretical accuracy of an angle calculated with the lsm6ds3 accelerometer.  From the spec I see there are a number of sources of inaccuracy/noise.  There is noise densi...

H3LIS331DL interrupt threshold

Posted on February 16, 2017 at 23:37hello,we are using H3LIS331DL to record shock on our instrument.we have setup INT1 to interrupt when acceleration>threshold.when the interrupt occurs we read out values and store it.we have observed that sometimes...

M24M02 I2C EEPROM Read Lock Status

Posted on February 16, 2017 at 15:48I am looking at the data sheet for the M24M02 and I want to read the Lock Status.  The data sheet says thisThe locked/unlocked status of the Identification page can be checked by transmitting a specific truncated ...

ttatakis by Associate III
  • 1078 Views
  • 1 replies
  • 0 kudos

LPS25HB questions

Posted on February 14, 2017 at 23:24We are evaluating the LPS25HB BP sensor, and have a couple of questions. I notice that several forum members have asked similar questions, but without receiving a reply. I would really appreciate an answer, as thi...

John L by Associate
  • 2347 Views
  • 3 replies
  • 0 kudos

LIS2DH12

Posted on February 14, 2017 at 13:03Hi all,I have got a technical question, if is possible to get some helpful feedback, I would really appreciate it, please.I have recently purchased a LIS2DH12 accelerometer and I am plugin it within a Teensy modul...

LSM9DS1.....Can someone please explain DEN_A/G pin? The datasheet mentions this pin once and does NOT explain whether it should be driven by host or not.

Posted on February 10, 2017 at 20:05The LSM9DS1 datasheet does not give a good description of the DEN_A/G pin.  Can someone add value to this?  Should it just be pulled high and never toggled by MCU?  Reference schematics of part from Sparkfun, etc....

swenner by Associate
  • 1001 Views
  • 1 replies
  • 0 kudos

WESU1 Clock Configuration issue

Posted on December 20, 2016 at 15:52hi all,     I have recently purchase a WESU1 device and used it as a reference for my custom wearable device design. i re flashed the WESU1 device with the sensor example firmware(STSW-WESU1) found it from followi...

LSM303D Interrupt

Posted on December 01, 2016 at 12:40I am having trouble getting the click interrupts to work for the LSM303D. using the library provided by Pololu for arduino I can get this code working for the DLHC[code]#include <Wire.h>#include <LSM303.h>long thi...