MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM303AGR magnetometer SET/RESET procedure

Posted on August 23, 2016 at 15:29Hi, I'd like to perform a SET/RESET procedure on the LSM303AGR magnetometer. As explained in the AN4825 pag. 17, if the user performs a single read, the bit OFF_CANC in CFG_REG_B_M must be set to '1' to invert the i...

marziano by Associate
  • 910 Views
  • 0 replies
  • 0 kudos

LSM6DS3 /LSM9DS1 fusion ref code

Posted on February 18, 2016 at 06:53Hello,I just wonder where i can get a referece code for fusion of gyro+ACCfor LSM6DS3 / LSM9DS1 

nir23 by Associate
  • 943 Views
  • 2 replies
  • 0 kudos

SPI communication with accelerometer H3LIS331

Posted on August 16, 2016 at 12:39Hi! I'm trying to read Who Am I register and get 0x32 reply from the accel. Not sure what SPI mode to use, 3? I see on the scope: byte 0xF1 come out of master on MOSI, eight clock cycles on SCK and SS line go low, b...

ot by Associate
  • 537 Views
  • 1 replies
  • 0 kudos

LPS25HB single point calibration after soldering

Posted on August 16, 2016 at 19:32I am trying to produce 6 matched sensors. I have soldered them and I can query them via I2C, but their values are significantly off true air pressure. I know I'm supposed to use the RPDS_L and RPDS_H registers, but ...

Problem linking in API VL53L0x

Posted on August 15, 2016 at 17:56 I am trying to use the API for VL53L0x proximity sensor over one smt32F4Discovery developement board and I am not able to do it. The steps that I am doing are the following: In a Keil project that it compiles ...

0690X00000603Q6QAI.jpg

LSM303D temperature sensor

Posted on June 13, 2016 at 14:41I could find the resolution of this sensor, 8 LSBs/DegC, but I couldn't find any information about how the absolute temperature is specified. Does anyone have more information about it? #ecompass #lsm303d #temperat...

kurt23 by Associate
  • 512 Views
  • 1 replies
  • 0 kudos

Reliability data for IIS2DH

Posted on August 10, 2016 at 15:35Is there any FIT and/or reliability data available for the IIS2DH accelerometer?

latise by Associate
  • 475 Views
  • 1 replies
  • 0 kudos

LSM303D temperature format

Posted on July 04, 2014 at 15:19Hello,I got good results reading accelerometer data but the temperature register is about 36 (decimal), the datasheet mentions 8LSB/°C, 36/8 = 4.5°C, this is quite cold ;) Room temp is 24°C, the other sensors locat...

tarzan2 by Senior
  • 581 Views
  • 2 replies
  • 0 kudos

LIS3DSH Temperature Output

Posted on July 20, 2016 at 15:35The LIS3DSH was implemented into one of our systems and currently we are having an issue with the Temperature readings across multiple units in the same environment vary from one another up to 15ºC. Is there a way to ...

LSM9DS1 Frequency Response

Posted on July 08, 2016 at 14:55Hi, We are looking for and 9 DOF sensor which should have good frequency response. I go through datasheet but was not able to fetch the frequency response details. Can you tell me the frequency responce of Part♯ LSM9D...

bimal by Associate
  • 632 Views
  • 1 replies
  • 0 kudos