MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS2DH12: do I need a different accelerometer?

Posted on February 28, 2017 at 00:33Hey,   In my application there is a lot of high frequency vibration that I am not interested in. The goal is to detect acceleration along a single axis that lasts 200ms or longer, but is generally between 1/2 and ...

How to detect click/double click with LSM9DS1

Posted on February 27, 2017 at 08:17Hello everyone,In the data sheet of LSM9DS1, it is stated in the first page that the device supports: Position and motion detection functionsClick/double-click recognitionHowever I cannot find anywhere in the...

Implementing Complementary Filter

Posted on February 24, 2017 at 20:11Hello everyone,To make this quick, I'm hoping to find any guidance on a particular issue we're having.We've developed a prototype wearable using ST's accel/gyro/magneto module. However we're trying to reduce the e...

LSM6DSL on IKS01A2 board won't put gyro data into the FIFO

Posted on February 23, 2017 at 08:04Hi all,I'm playing with the LSM6DSL sensor on the IKS01A2 board.I'm trying to use the FIFO to record and buffer accelerometer and gyro data.The accelerometer works fine and reading the gyro registers directly give...

Half sensitivity of one VL53L0X

Posted on November 07, 2016 at 11:56Hy,for a proof of concept I created five identical devices, each having 3 VL53L0X, so I have an overall of 15 VL53L0X that are mounted (behind an acrylic glass shade) and connected (via 2.8V, I2C) identically. Dur...

harald by Associate III
  • 702 Views
  • 2 replies
  • 0 kudos

Is the LSM6DS3H and LSM6DS3US the same part?

Posted on February 22, 2017 at 02:00I have went to just order the H version and found there is none left. Anywhere. So then I started looking and the US version is on stock. All the specs look identical but I just want to know for sure. Any help or ...

curtis2 by Associate
  • 933 Views
  • 1 replies
  • 0 kudos