LIS3DH ADC Specifications
Posted on October 30, 2013 at 03:02Are the specs for the ADC in the LIS3DH available? I'm particularly interested in input voltage range, input current, and recommended capacitance for ADC inputs.
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Posted on October 30, 2013 at 03:02Are the specs for the ADC in the LIS3DH available? I'm particularly interested in input voltage range, input current, and recommended capacitance for ADC inputs.
Posted on April 08, 2014 at 16:13Hi,Is there an easy way to 'factory reset' the LIS3DH?Does a simple power cycle do this?I looked through the data sheet and app note and could not see this defined there.Thanks #lis3dh-reset
Posted on October 04, 2016 at 12:47Hi How can I start with LIS2DH12 accelerometer programming , is there any tutorial for beginners about the registers ,how they work and how to write a program for them ? hanks for help #accelerometer-lis2dh12-c...
Posted on September 30, 2016 at 07:49Does anyone know how to change the standard mode to 2V8 mode?I could not find the details in the VL53L0X API manual. #vl53l0x
Posted on October 03, 2016 at 18:03Hi, in datasheet for LPS25HB ('DocID027112 Rev 3'), page 27, the register 'RES_CONF (10h) Pressure and temperature resolution' is described. Question1: Is the 'Nr. internal average' (table 18) applicable for One-sh...
Posted on October 03, 2016 at 16:26where can I download iNEMOEngine_LI3 source code. I can't find a link to it
Posted on October 03, 2016 at 12:51Distance measured by the sensor is direct value or averaged value? If it is averaged value means then in what way they are averaged ? Is FOV takes major role in averaging?
Posted on September 27, 2016 at 15:34I am using the L3GD20H in an application where I am measuring the angular velocity of a pendulum. I want to calculate as accurately as possible the kinetic energy. I have calibrated for gyro zero-offset drift, ...
Posted on July 19, 2016 at 21:00I had already multiple times the problem that the accelerometer sensor is not providing data anymore. It is connected via SPI, commands like the who_am_i works, however the XYZ data is all zero or just some frozen val...
Posted on April 21, 2015 at 17:00Hi I'm just bringing up a VL6180x mounted on a VL6180X-Satellite board with bit banging software. Everything has gone well so far, writing and reading registers etc, for proximity only application. The ranging output...