MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LPS22HB Attach process Flux

Posted on November 16, 2016 at 17:25Which flux is best for attachment of this product?  Is this device susceptible to damage if cleaned using an aqueous wash?

stst9182 by Associate
  • 400 Views
  • 0 replies
  • 0 kudos

LIS3DH high-pass filter not working

Posted on March 16, 2015 at 07:14At work I am using the LIS3DH accelerometer to detect body motion.  It is configured for +/-2 gs, 50 samples per second, with Streaming FIFO.  The watermark works fine for determining when the FIFO needs to be emptie...

microbob by Associate
  • 820 Views
  • 2 replies
  • 0 kudos

Can be use accelerometer for Vibration measurement?

Posted on November 09, 2016 at 07:32I am using LIS332AR mems chip for vibration measurement. Assembled this chip in PCB and PCB located vertical with respect to ground. For every 90 degree rotation of this chip corresponding X and Y axis value chang...

LISDH12 high consumption

Posted on November 03, 2016 at 17:34Hi all,i use an accelerometer  LISDH12, and it have a very high consumption (400 uA).I have this configuration; SCL/SDA connect to vdd with 4.7kCS to high because i want to use a i2cSDA0 put on groundSomeone hav...

anna by Associate
  • 747 Views
  • 3 replies
  • 0 kudos

MKI109V2 motherboard firmware upgrade

Posted on November 09, 2016 at 20:03Hi,I just got new MKI109V2 motherboard, and installed the driver for DFU and VCP. At the beginning, I can detect VCP on my PC and use DFU DEMO to upgrade firmware. After upgrading firmware DFU_Patcher_V1.0.2.dfu, ...

ljin by Associate
  • 548 Views
  • 1 replies
  • 0 kudos

LSM303AGR Acclerometer jerk detection

Posted on November 06, 2016 at 07:50Hi I am planning on using LSM303AGR to detect a jerk in my system. And I want LSM303AGR to send an INT1 to the CPU to wake.I am thinking to use the accelerometer to determine this jerk. Magnetometer will be in sle...

toashwin by Associate
  • 491 Views
  • 0 replies
  • 0 kudos

LSM303AGR Arduino based Examples

Posted on November 06, 2016 at 07:43HiI am thinking of using LSM303AGR I2C interface. Are there any Arduino based examples for this product?I could not find any online.Thanks #arduino

toashwin by Associate
  • 429 Views
  • 0 replies
  • 0 kudos